Hi,
I am facing one issue in my circuit.Issue is-
My board is working at 12V input. I am using fuse at the input side of 3A current rating.
As soon as I powered up the board, the fuse is getting burn(in some board).If I remove the fuse and short the board then the circuit is working fine and taking the current as same in the working board(having fuse)
I checked the impedance of the board and it is fine.
I replaced the fuse of the working board with this board then also it got burnt.
I am not able to debug the issue.Please help.
Thanks
Ash