I have two questions for LM43602.
1. For soft start, how much is the maximum value of the time with SS pin open?
Is the value lower than 10ms? I understand the specification is not guaranteed, but I would like to
confirm whether the value is lower than 10ms or not, because the customer need less than 10ms.
2. For operating quiescent current, how much is the maximum value of the current?
I understand the specification is not guaranteed too, but the customer want to know the approsimate
value.
Best regards,
Atsushi Yamauchi