A datasheet has the following statement.
It is important to ensure that a valid input voltage (2.8 V ≤ VIN≤ 5.5 V) is present on the VIN pin before the EN input is asserted.
The demo board is a resistor divider to pull EN pin up to half Vin.
So the IC will be enabled when VIN is higher than UVLO(typ 2.55V), but EN pin is 1.275V then.
I think EN pin is asserted before VIN reached a valid input voltage.
Doesn't this become a problem?
Please tell me the correct divider value in the case of 3.3Vin?