Hello,
We have designed a DC/DC converter using the LM3150 to generate a 2A 13V power rail from a 24V Lipo battery. This 13V power rail is used to feed an external load (pump) and to generate all the system power rails (10v, 5v and 3.3v).
When we test this solution with a laboratory power supply, results are good : we have an output voltage of 12.9V and we can deliver 2A to the external load and supply all other system power rails without heat increase or output voltage drop. We made the test with input voltage values from 20 to 32V.
Problem is if we feed the system with the Lipo battery (@ full charge Vbat = 28.8V), the LM3150 is irremediably destroyed (component explosion with smoke). We have performed the test on 2 boards with same results.
please find the schematic of the LM3150 power stage.
6545.SCHEMATIC1 _ Power Supply.pdf
I hope someone can help me to find a solution !
Thanks,
Eric