Hello,
I have tried to use two LMR14203 do generate +5V and +18V from a 24V to 36V source. The design was made with Webbench. By reading through related posts in this forum I understand that the layout is not optimal and trace width to the diode and inductor should be increased. However, I don't understand why the circuit does not work at all. On top of that the two subcircuits react differently. The schematics and top layer of the PCB are shown in the attached file. The design is a two layer PCB with a ground plane below the switching circuit.
The 5V circuit does not show any output voltage when used with 25V input. Also no feedback voltage can be measured which is kind of obvious as there is no voltage at the diode or inductor.
The 18V circuit shows different voltages depending on the input voltage. Typically the output voltage is 2 or 3 V below the input voltage. There is however no sign of any switching at all. When measured with the scope on the diode or the inductor only a constant voltage can be observed.
I should mention that there is a 110uF capacitor in parallel with the input voltage. The measurements and the tests have been made without load and in the circuit the load will be rather small.
Any hints are greatly appreciated.
Thanks