Hello All,
I have designed a step-down converter using LM46002 with following parameters:
Vin: from 14 to 22 volts
Vout: 3.3V
Iout: 2A
In schematics I got maximum voltage of Cboot is 35V but in datasheet for LM46002 absolute maximum ratings between BOOT and SW pins is only 5.5V. Mistake in Webench?
Best regards,
Nikolay Gavrikov