Dear Sir/Madam,
I am using LMR14030SDDAR (8 pin SOIC) power supply IC in my prototype project.If everything is fine i need to immediately go for mass production. My input will be 7.5V to 36V and i have design to get an output of fixed 5V. But the output is already only 4.7 to 4.8V. From this i will be generating 3.3V, 1.2V, 8V.Since LMR IC supports and output current of 3A.With 3.3V only enabled the performance is OK, but when i start using 1.2V the 5V output is unstable and 5V drops down to 4.5V or less. Please help me out. I have nearly followed the same design as the EVM board. If needed i will share the schematics of the power supply section with you. This is very critical phase of the project.
Thanks and Regards
Shankar.R