Hi,
I encounter an issue in power system design, enclose is the schematic design of LMR12010 20Vin,1A step down voltage regulator.
The issue is I can’t get the correct output voltage(3.3V) while I having 12V input voltage, below is my part list.
C18 – 10uF 25V
C19 – 0.01uF 25V
C20 – 10uF 6.3V
R6 – 100k ohm
R7 – 31.6k ohm
R8 – 10k ohm
L1 – VLCF5028T-2R7N1R8-2, INDUCTOR, 2.7UH, 1.82A, 30%
D2 - MMSD4148T1G, diode
http://www.onsemi.com/pub_link/Collateral/MMSD4148T1-D.PDF
D3 - MBRA120TRPBF, Schottky Diode
http://my.element14.com/vishay-semiconductor/vs-mbra120trpbf/diode-schottky-1a-20v-sma/dp/8660409
U4 – LMR12010
http://www.ti.com/lit/ds/symlink/lmr12010.pdf
Please kindly advise us on this issue.