Hello,
I've been trying to configure the LM2678-ADJ simple switcher to be either controlled by a PWM or DAC signal. The schematic in the picture is the circuit I'm currently using to do this with. I have tried feeding the DAC signal in through the GND side of R6(1)1 but the reference voltage of 1.21V will increase to about 6V and the LM2678 dies. I got this idea from how the LM317 output can be controlled by changing the GND reference for its resistor divider.
I decided to try a summing method which is what you see here in the schematic. The idea is that as the voltage from the DAC or PWM increase the output decrease. This seems to work to a point, but then stops as described in the comments on the schematic. I'm having trouble trying to understand why I'm getting this behavior and solving the problem. Any help on the matter would be great. If you need further information please don't hesitate to ask I'll do my best and respond as soon as possible. I look forward to hearing from you.
Regards,
Lee
Spec info: Switcher input is around +33V DC, Op-amp rails +12V DC, -12V DC, and MCU is powered by +3.072V DC