Hi,
I would like to know if we can do an application similar to the below with one of our LMR or Simple Switchers in general.
Thanks
Umberto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to know if we can do an application similar to the below with one of our LMR or Simple Switchers in general.
Thanks
Umberto
There are a few concerns with this topology.
The circuit shown in the attached PDF (page 34) states the input range is 4.5V to 28V, but the FET Q1 gate drive voltage is rated up to 16V. If Vin is above 16V, Q1 will be damaged. Be careful with the Vin range in your application.
The buck-boost topology has different loop response than a buck topology. This application idea did not provide how to properly calculate the type III compensation network so that it is stable with the buck-boost topology. The LMR14020 has internal compensation network for ease of use. The compensation network is not tested in the buck-boost configuration.
The inductor in the buck boost topology conducts much more current than it is in a buck converter. Be careful with the current rating of the inductor if you decide to proceed with this topology.
Hope this helps.
Yang
Hi,
Yes, we did similar reference design before. Here is the PPT.Positive Buck-boost Converter .pptx