Hi,
We are working on a project where we use Delay Superviser TPS3808G09DBVR for voltage monitoring. We used dot matrix board and when we left the Ct pin floating, we got the reset output with fixed delay. When we tried with ct pin pulled up to 51k ohms, we got the reset output with fixed delay. But when ct capacitance varied from 1nf to 390pf, no consistent output is observed as in below table. Please help to resolve the issue
Capacitance Ct |
Calculated Delay (ms) |
Measured Delay(ms) |
1nF |
6.2ms |
30ms |
680pF |
4.4ms |
No O/P |
390pF |
2.7ms |
5.4ms |
218pF |
1.74ms |
No O/P |
150pF |
1.35ms |
No O/P |