Hello guys,
One of our customers is considering using TPS3813.
They have the following questions about the device.
Could you give me your answers to the questions?
Q1. On page 10 in the device datasheet (SLVS331H), we can see the sentence, "The TPS3813xxx family of devices have a watchdog timer that must be periodically triggered by either a positive or negative transition at the WDI pin to avoid a reset signal being issued." Does this sentence mean that WDI rising edge and falling edge, both edge are detected as a valid signal for watchdog timer resetting?
Q2. If WDI falling edge is input before t_boundary,min is elapsed, is this valid and does /RESET level go low? (I think the answer should be NO because the falling edge is input before t_boundary,min is elapsed according to Fig 1, Timing diagram.)
Q3. If WDI falling edge is input after t_boundary,max is elapsed, does /RESET level not go low? And then is WD timer reset?
Q4. Is the rising edge of WDI only is detected until t_boundary,min is elapsed?
Q5. Must the falling edge be input by t_boundary,min is elapsed?
Your reply would be appreciated.
Best regards,
Kazuya Nakai.