Other Parts Discussed in Thread: TPS3710, TPS3847
Hi,
Our application requires a UVLO monitoring IC similar to LM8364 but with a wider input voltage range up to 12V or 14V.
The threshold we are looking is around 2V.
And also it is mandatory to have an output(/RESETpin) at the ground when the system is powering ON.
Can anyone suggest a suitable substitute for LM8364 to meet the above requirement?
I have gone through the TPS3710, but it cant predict the output until VDD ramp above 1.8V.
Thanks in advance
DEEPAK V