Hello dear Ti community.
I've got a dual rail power supply which will power up my amplifier.
Both of them got enable PIN (TPS7A4701 and TPS7A3301) so I want to use them better than with simple voltage divider which is not enough in my case.
What I'm looking for? I'm looking for a simple solution to monitor both negative and positive voltage which will be presented at regulators input pins.
It would be nice to achieve one thing, lets assume that one of power rail will go down below 20/-20V (I've got both regs adjusted to symetrical 18V) if that happen one of two regs will be off till malfunction will be removed. I'm looking for a solution that will turn off both regs even if one of them can be properly powered up, no matter which voltage will be below threshold (pos or neg).
I never done that before so I'm looking for a solution, IC proposition etc. I neved had that kind of issue in the past, but it would be nice to be protected anyway :)