Part Number: UC2903
I need to monitor +15V & -15V opamp power supplies. I'm having some difficulty understanding the concept behind sensing a negative voltage level using SENSE 4 & SENSE 4 INVERT INPUT lines.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UC2903
I need to monitor +15V & -15V opamp power supplies. I'm having some difficulty understanding the concept behind sensing a negative voltage level using SENSE 4 & SENSE 4 INVERT INPUT lines.
Vijay,
Figure 6 shows how to configure the device for negative voltage sensing. The idea is to use the internal comparator that is set in the inverting configuration. Pin 5 is the inverting input and connected to ground because Pin 3 is GND. So by applying a negative voltage across R2 with the negative side on the bottom and the positive side at Pin 5, this will detect negative voltage. The negative voltage is scaled using R1/R2 * 2.5V.
Please let me know if this is clear.
-Michael