Hello,
i am using the UCD90160 to monitor eight voltages and their currents. I am using shunt resistors and INA197 OpAmp to measure current scaled to 2.5V max. input voltage for the UCD90xxx ADC. Why is the current and temperature assignment on the Pin Assignment tab in Fusion Digital Power Manager Software not available for UCD90160 device? Starting a project with the UCD90120 showed that the current and temperature assignment options are available for that device.
Are there any main functional differences between the UCD90120 and the UCD90160? I couldnt find any on the datasheets.