Other Parts Discussed in Thread: TPS1H100-Q1
Hi,
My customer is using TPS1H100-Q1 and TPS4H160-Q1.
He do the transient voltage test, JASO D001-94 D-1,
He did implement a surge absorber on his board, then he could clump this surge voltage under 60V.
But maximum absolute rates of datasheet shows 48V(t < 400ms).
In addition to above spec, Is there the spec for the transient voltage test of JASO D001-94 D-1?
I show the transient voltage test, JASO D001-94 D-1 below.
Best regards,
Shimizu