Hi,,
I am using the TPS2H160 to provide overcurrent protection on a 28V power rail.
Both channels of the device are wired in parallel and the current limit is set to a value of 1.68A (each output set to 0.83A).
I have noticed that when I slowly ramp the load current, the device actually trips at 2.2A which is greater than the quoted +/15 % in the datasheet..
The same part in a similar application programmed to a trip current of 2.2A also trips higher than expected (~3A)
The circuit is shown below. The load is an electronic load set in constant current mode connected to the same ground.
Any help is appreciated