Team-
Page 8 of the TPS25942 data sheet provides the min/max thresholds for V(REVTH) as -15 mV and -3 mV respectively, and a typical value of -9.3 mV.
How many standard deviations are implied between these min/max values? +/- 3 sigma? +/- 4.5 Sigma? +/- 6 Sigma?
We have a problem where the back-feed current necessary to turn off the device is getting too high and we need to better understand the statistics around this parameter to solve the problem.
Essentially, given that Rds,on can be as low as 26 mOhm, this implies that the device will not isolate until a current of 15 mV/26 mOhm = 0.576A flows backwards through the device, worst case.
Using typical values, we would expect 9.3 mV/42 mOhm = 0.221A to be sufficient.
We need to understand the probability of currents exceeding about 350 mA; obviously, the lower the back-fed current, the better.