Dear Specialists,
My customer is evaluating TPS22902YFPR and encountering problem.
Could you please advise?
---questions
I am evaluating TPS22902YFPR, some samples are not working correctly.
When the device is power ON and Switch control is OFF, Vout pin is output.
Could you please see attached files.
Are these proper operation or broken?
If the devices are broken, what is the reason?
Is there any problem in the circuit.
<The circuit condition>
(1)A load resistance is 150kohm, and then divided and connected to A/D converter.
(2)ON/OFF control voltage is 3.3V from CPU.
(3)Input power supply is 3V battery 15mAh, and then 390ohm, and then connected 3.1V LDO.
(4)When the main power is off, TPS22902 is powered from battery and ON/OFF control become Hi-Z
---
I appreciate your great help.
Best regards,
Shinichi