Hi All,
Please find the block diagram with active component configuration below:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
Please find the block diagram with active component configuration below:
Hi Rakesh,
Thanks your reply.Forgot to attached both block diagram and captured waveform.
Please find the block diagram with passive component value below:
Captured waveform below
we are facing glitch issue on EN signals.
why EN glitch is coming on EN signals?if anybody faced similar issue,Please let me know how to solved it.
Thanks & Regards,
Anandraj.S
Thanks for your reply.
We have changed the R1 = 100K and R2 = 19K6 in our board, now glitch is reduced.
As per the datasheets, under voltage lock set point formula below:
Vuv=((R1+R2)*VENR)/R2 where VENR-=1.4V
Captured waveform with configuration (R1 = 100k ;R2 = 19K6 ;VENR =1.4V) below:
Theoretical value of under voltage set point (Vuv) = 8.542V.but measured value is 9.72V.
1.Why under voltage set point of theoretical value (8.5V) and measured value(9.72V) are not matching?
2. Recommended Max current on EN pin?
3. Please suggest the values for the configuration below:
Vin = 12V;
under voltage set point Vuv=10V.
current limit thersold limit =3.7A
Setting the output ramp time =2.6ms
R1=?;R2=?;CdVdT=?;RLIM=?.
With Thanks & Regards,
Anandraj.S