Dear Specialists,
My customer is considering input circuit of TPS4H160-Q1
I would be grateful if you could advise.
---
Depending on the usage conditions, the voltage input to the logic of Input fluctuates considerably.
Since the rated voltage of Input is 7 V, it is necessary to clamp the voltage with a Zener diode or the like, but I do not want to increase the number of elements anymore.
So, I am thinking a method like the attached file.
Please tell us your opinion whether such use method is problem.
---
The customer' d like to obtain the reply as soon as possible.
I appreciate your great help and cooperation in advance.
Best regards,
Shinichi