I am attempting to measure Ls' but am struggling and need some help. The Qi spec describes a test environment for performing this measurement and that description is also described in the bq51013A datasheet from TI. I am trying to follow it.
I have a transmitter coil from a TI evaluation module bq500212AEVM. I unsoldered the Tx coil and am driving it with a function generator and sine wave, 100kHz and 1Vrms. I have provided the 3.4mm dz spacing. My mobile device has a metal plate and battery, etc, so I assembled my entire mobile device and drilled two holes to bring the two coil wires out of the case for measuring Ls' with an LCR meter.
The L reading is stable when the Tx is not present but the L reading bounces all over the place when I am running the sine wave through the transmitter. What might be going on with my setup?