I have no understood when I have to use 4.1V, 4.2V or 4.36V.
I mean, in which situation is it important to have a power charger that fit exactly these voltages?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have no understood when I have to use 4.1V, 4.2V or 4.36V.
I mean, in which situation is it important to have a power charger that fit exactly these voltages?
Gianluca,
The choice of 4.1V, 4.2V and 4.35V is based on the battery chosen and indicates when the battery is considered full. The charger will terminate charge when that voltage is met.
You need to base the charger on the specification of the battery.
Regards,
Dick