Dear TIer,
Datasheet of BQ51221 describe Pull High to enable CM_ILIM as below. But under the 5th line, Pin high to diable CM-ILIM. What is the right operation of CM_ILIM?
"The communication current limit can be enabled by pulling CM_ILIM pin high (>1.4V) or disabled by pulling the
CM_ILIM pin low. There is an internal pull down that enables communication current limit when the CM_ILIM pin
is left floating. When the communication current limit is enabled, the amount of current that the load can draw is limited. If the charger in the system does not have a VIN-DPM feature, the output of the receiver will collapse if communication current limit is enabled. In order to disable Communication Current Limit, pull CM_ILIM pin high."