Hi
My customer is using BQ51050B.
Q1, He wants to set TS range from 3 degrees to 43 degrees.
In this case, I think that he should calculate R1 and R3 by (3),(4) in datasheet.
then parameter is the following.
Is my idea correct?
%Vcold = 58.7, Tcold = 3
%Vhot = 13.1, Thot = 43
*Refer to NTC resister datasheet about another parameter .
Q2, ERT-JZEG103JA as example is suggested in Figure26 of datasheet.
This B value is 4500.
But I confirmed that B is 3435 in ERT-JZEG103JA datasheet.
Which value is correct?
Thanks
Shimizu