Hello,
I am using BQ51050B receiver chip with the TESLA demokit and I am trying to find out what happens to the lost energy in the transmission. Since I use battery charging current of 100 mA (chip can deliver up to 1A) the overall efficiency is very low ~30%.
1) Is the energy radiated? (If we use smaller receiver coil comparing to transmitter one, are there radiative losses?)
2) Is it lost in the rectifier at the receiver side or some other component?
3) Or is it jsut a resistive loss in the resistor which we use to determine the battery charging current.
Do you have some study related to this topic? Did you measure overall efficiency in TIDA-00318 reference design?
Thank you very much for help,
Radoslav