Hi ,
I have got the wireless charging system based to work ( bq500212a Tx and bq51050b Rx). when the Rx was set for 650mA charging current i had no problem regarding the start of charge, as soon as i bring the rx close to the Tx the charging would start. i recently changed the settings to 900 mA usinf R=110 and R2=220 ohms. right now am havnig problem getting the charging to start but once it starts everything is fine . if i move the Rx a little or remove it and put it back on the Tx the charging doesnt restart or sometimes it does after some time. i wonder what coul be the reason behind this. i have charged two batteries at 900 mA and everything works well once the charging starts
Thanks