Hello all,
I am currently working with the BQ25504EVM, an eval module that takes in a low-voltage DC signal (from an energy harvester) and boosts/regulates the output voltage. The BQ25504 device itself has an output voltage range from 2.5V-5.2V, however, the eval module is factory programmed (via voltage dividers) to output ~3V.
My design goal is to charge a battery from the eval module.
1. So, WHY did they choose to make the output of the eval module 3V? It is marketed as being compatible with multiple battery chemistries, but many of the common rechargeable batteries need at least 3.7V-4.2V to charge, which this evaluation module cannot provide.
2. Are there any specific rechargeable batteries (or chemistries) that can be charged off of 3V? I have looked around and cannot seem to find anything.
Since I would like to get a higher voltage out of the device, I intend to design my own PCB for it. The BQ25504 datasheet contains a few sample schematics. However, the voltage divider equations that govern many of the output voltage thresholds mention a "VBIAS" in their equation, which really isn't mentioned anywhere else in the datasheet, and also does not appear on any of the schematics.
3. What is VBIAS referring to? How can/should it be controlled?
Thanks,
Matt A.