HI,
I'm having trouble understanding the math required for R1 and R3. Can someone please clarify????
I tried going through the example on the datasheet, Page 25 and 26, but I do not understand the math for values for R1 and R3.
My process:
1.) I calculate R,NTC|COLD and R, NTC|HOT using the following...
This equates to roughly,
R, NTC|COLD = 28.224 kOhm
R, NTC|HOT = 3.039 kOhm
2.) This is where I'm confused. Using equations 3 and 4 from the datasheet page 25, I try solving for R1 and R3.
Where R2 = 20kOhm as stated in the circuit from above.
Based on the Electrical Characteristics table from page 8, I use the values of 58.7% and 13.1% as my %V, COLD and %V, HOT respectively.
I'm not sure what to do after this.
What I know,
If R3 is significantly larger than R1+RNTC or R1 is significantly smaller than RNTC, then one can remove R3 and R1 respectively I do not wish to have an R3 value. Do I just set it to 1MOhm and work the equation that way???
Someone, please clarify. It would be appreciated if you showed the maths.
Thank you,
Mauricio Solis