Hi,
I am setting up two DMA channels (Tx and Rx) to test through McBSP with DLB. For some reasons, there is no EVENTs happening.
What might be the problem? Do you have some example code doing EDMA3 with McBSP for C6657?
Thank you.
Regards,
Steve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am setting up two DMA channels (Tx and Rx) to test through McBSP with DLB. For some reasons, there is no EVENTs happening.
What might be the problem? Do you have some example code doing EDMA3 with McBSP for C6657?
Thank you.
Regards,
Steve
There should be some example code coming out with the next release of the PDK which includes the McBSP drivers.
We'd need a lot more details regarding your McBSP and EDMA configuration to know where to start debugging suggestions.
Best Regards,
Chad
I'd start with how the McBSP is configured (all the details.) How the EDMA is configured all the details (Setup as FIFO or incremental SRC/DST, etc.) What you're observing at each step, did the PaRAM entry from the transfers (both TX and RX) get consumed (i.e. are they now updated w/ a null transfer.)
May want to provide the source code as well.
Best Regards,
Chad
Hi Chad,
The following are McBSP register settings at end of configuration.
I set them in this order: SPCR=0 // reset.
Then PCR, RCR, XCR, SRGR and SPCR.
The following is EDMA3 PaRam settings:
Then, I call: result = EDMA3_DRV_enableTransfer (hEdma, tx_chId, EDMA3_DRV_TRIG_MODE_EVENT);
result is 0. But nothing happens, no change in the PaRAM.
Thank you.
Regards,
Steve
Steve,
It sounds like you haven't triggered the event yet to begin the transfers. Have you looked at event 64 (the event associated with the PaRAM entry @ offset 0x4800)?
Best Regards,
Chad
You've only setup the McBSP to transfer data, it needs to be feed by the EDMA. You need something to trigger it. In this case, I'd just use the ESR (event set register.) This is documented in the Keystone EDMA3 UG. Which can be found on the TMS320C6657 product page.
Best Regards,
Chad
No, we don't have example code for this particular scenario. You need to have the McBSP trigger the event for the receive EDMA transfer, it should then trigger the transmitt transfer, etc. You really haven't tied the McBSP and the EDMA setups together. The EDMA is dependent on events triggering the transfers.
Best Regards,
Chad
Chad,
You are right. I also feel that the event trigger is not working. Because McBSP1's DXR never change. Not like when I use CPU to write DXR, the data show up right away.
I used DXR as EDMA's transmit destination which is address: 0x21B8004. But in EDMA3 User Guide (SPRUGS5A)
"2.3.2.3 Channel Destination Address (DST) The 32-bit destination address parameter specifies the starting byte address of the destination. For DAM in increment mode, there are no alignment restrictions imposed by EDMA3. For DAM in constant addressing mode, you must program the destination address to be aligned to a 256-bit aligned address (5 LSBs of address must be 0). The EDMA3TC will signal an error, if this rule is violated."
But ERRDET is 0x00000000, signal no error.
What address should I use, if 0x21B8004 is illegal for EDMA3?
Thank you.
Steve
Set it to incremental mode for both TX and RX. You're doing a 4-byte transfer and you need to fill the 32b register with the data. With the Destination Index Increment set to -4, it should snap back to the same spot.
-Chad
Ok, I'm going to ask one of my team members to step in here and take a look.
Best Regards,
Chad
Steve,
We need to use specific EDMA channel for the transfer which are being triggered by McBSP events. Please refer to Table 7-32 in C6657 data manual. Channels 36~39 are for McBSP0/1 receive/transmit events.
I also attached one example project to demonstrate the McBSP/EDMA setup. The attached has some McBSP CSL files which is ported from other device, not existing in the current C6657 PDK packet. As Chad said, the next PDK release should have some McBSP driver for the configuration. The current attachment is just one example for reference.
Please also note the McBSP have both non-FIFO and FIFO modes, The DXR and DRR addresses are different in those modes. Please refer to the C6657 memory map table for details. The example code should show the difference as well.
Hope it helps.
Hi Steven,
Thanks for the infomation and example code. I ran the example code and found the following.
The transfer only happen once per power cycle. Here is the procedure:
power cycle,
load code and run, transfer works (rx buffer changed to tx data) for none FIFO; transfer also works for FIFO.
restart and run, transfer doesn't work, rx buffer stays all zero.
What might be the problem?
Thank you.
Steve
Hi Steven,
After more testing, 4555.McBSP_EDMA_example.zip code only work by running from Restart to finish. If stepping through, tx buffer to rx buffer copy will not happen. And also, the board needs to be cold reset to work again.
Your explanation is appreciated.
Thank you.
Regards,
Steve
Steve,
Have you loaded the C6657 GEL file to do "Global Default Setup" to initialize the EVM please?
Another possibility is that there could be some residue in EDMA/McBSP setup with L1D/L2 cache enabled, which requires the reset for put the EDMA/McBSP into default states.
So I added some code in the beginning to disable L1D/L2 cache in the example and I tried the output file on C6657 EVM that it could be re-run without cold reset or even hot reset. Please give a try on the attached example.
Hi Steven,
Sorry for the delay. I was on vacation last week.
I tried your 1106 code and it worked pretty much the same way. After more testing, I discovered the following:
With a fresh start, I can repeatedly run from startt to finish (restart after each run) without problem.
If I set break point in or immediately after these code, then system needs to be cold started to operate correctly again. Note: ipr.intrh become 0x00A0, not 0x00F0.
Tx_Rx_Clkgen_Frmgen(hMcbsp[0], MCBSP_ENABLE); /*Enable TX, RX, SRGR clock and SRGR Frame generation */
Tx_Rx_Clkgen_Frmgen(hMcbsp[1], MCBSP_ENABLE);
VAL_TRACE(0x99990000);
do {
CSL_edma3GetHwStatus(hModule, CSL_EDMA3_QUERY_INTRPEND, &ipr);
} while(ipr.intrh!= 0x000000F0);
Thank you.
Regards,
Steve
Steve,
I think it is due to the emulation mode in McBSP. By default, the FREE and SOFT bits in SPCR register are 0s. The McBSP TX/RX will stop immediately when you reach the breakpoint (an emulation suspend event). Then the EDMA channels will not be triggered by McBSP events, so the flag checking (ipr.intrh) is stuck.
If you want to keep McBSP running during emulation event, you can set FREE bit to 1 in SPCR register during the McBSP initialization. Please refer to section 2.16 in McBSP user guide for emulation details.
You can make the change in the example and let us know if it is working for you.
Hi Steven,
The EMDA3 and McBSP seemed work fine with your sample code. I am try to look at the signals on McBSP lines at TEST_PH1 connector, pin 76 (Tx data), pin 72 (FST) and pin 66 (TXCLK). The data looks good. But the frame sync and clock seem has contention. See scope capture below.
Thank you.
Steve
Hi Steven,
I found the problem with the issue above. TMDXEVM6657L's FPGA is contenting with clock and frame sync. We need to configurate FPGA registers that are accessed through SPI. Do you have sample code to read/write SPI on C6657?
Thank you.
Regards,
Steve
Hi
Which board is this code being tried on? I am also trying on the TMDXEEVM6657 board. It just hangs at
CSL_edma3GetHwStatus(hModule, CSL_EDMA3_QUERY_INTRPEND, &ipr);
I also included the FPGA code and set
/*Write FPGA Register*/
uchValue = uchValue | 0x03;
ret = fpgaWriteConfigurationRegister(0x0c, uchValue);
Regards,
Hari
Hi Jari,
I am using TMDXEVM6657L board. I also had code hanging at
CSL_edma3GetHwStatus(hModule, CSL_EDMA3_QUERY_INTRPEND, &ipr);
whenever I step through or set break points around the code before this line. If you cold reset your board and run without break point, you should run through and pass all the tests. I suspect that the problem is due to McBSP/EDMA3 encounters emulation stop. Even with setting for stop/continue run with emulation halt, it never worked. Could you do some research on how to get McBSP/EDMA23 running with emulation stop? So I can debug this code.
Thanks for the info on write FPGA registers.
Regards,
Steve
Steve,
In my case, even after the following steps It hangs at GetHWStatus()
- power on
- connect USB
- open CCS project
- Press the DEBUG Icon (green)
- It runs GEL loads the .out file. Goes to MAIn().
- Simply run without break points.
- HANGS at the GetHWStatus (EDMA polling)
- Stop
Power off/on
- repeat
- HANG
I do not see any difference. Only difference is there is no suffix 'L' on my board it is TMDXVM6657
Steve,
Regarding to the breakpoint issue, I made some changes in the source file, basically we
1. enabled the free run in McBSP
//mySetup.emumode = CSL_MCBSP_EMU_STOP;
mySetup.emumode = CSL_MCBSP_EMU_FREERUN;
2. initialized the ipr variable before reading from the EDMA register
ipr.region = CSL_EDMA3_REGION_GLOBAL;
ipr.intr = 0;
ipr.intrh = 0;
3. and added some delay between initialize McBSP and enable McBSP
for(k=0; k <= 50; k++); //adding delay
Then I made the breakpoints in or after the section you mentioned before, I was always seeing iprh=0xF0, (not 0xA0).
Tx_Rx_Clkgen_Frmgen(hMcbsp[0], MCBSP_ENABLE); /*Enable TX, RX, SRGR clock and SRGR Frame generation */
Tx_Rx_Clkgen_Frmgen(hMcbsp[1], MCBSP_ENABLE);
VAL_TRACE(0x99990000);
do
{
CSL_edma3GetHwStatus(hModule,
CSL_EDMA3_QUERY_INTRPEND,
&ipr);
}while(ipr.intrh!= 0x000000F0);
Please give a try with the update in the attached file and see if you it works for you.
Hari,
You can give a try with the new source file as well. I do not see the test case hang like you described. Probably you can check the power/clock in your setup, if using the correct GEL to do global initialization, or try another EVM. And check the EDMA (IPR/IPRH) or McBSP registers to see if they are being properly programmed as we plan to do in the test case.
/*****************************************************************************\
* TEXAS INSTRUMENTS INCORPORATED PROPRIETARY INFORMATION
*
* Property of Texas Instruments
* For Unrestricted Internal Use Only
* Unauthorized reproduction and/or distribution is strictly prohibited.
* This product is protected under copyright law and trade secret law
* as an unpublished work.
* Created 2011, (C) Copyright 2008 Texas Instruments. All rights reserved.
*------------------------------------------------------------------------------
* Filename : tput_search_128ch_32bit.c
* Date Created : July 21, 2011
* Last Modified :
* Description : Checks the throughput of McBSP by running the testcase at
* different clock frequencies and records first frequency
* the test case fails. McBSP transfer requests are routed
* through Config bus.
* History : Ported from CURIE
* Project : Gauss
* Author : Kanchana
\*****************************************************************************/
/* ** \Register Configurations:
** -# No Of Phase - 1,
** -# Word Length - 32,
** -# Frame Length - 128,
** -# Data Delay - 0,
** -# Interrupt on Mcbsp Transmitter and Receiver SYNC Error conditions.
EDMA Interrupts for Event Completion.
** -# XCLK --> RCLK, Internal XFS --> RFS
** -# Loop Back Mode - DLB ON,
** -# Internal Frame Sync Generation from Sample Rate Generator
** -# Frame Sync Pulse Width - 1,
** -# Frame Sync Period - 0xFFF for 128 Channels,
** -# Clock Divide Value - Variable,
** -# Enhanced Multi channel selection Enable (128 Channels)
** -#First run with FIFO disabled(CFG path), then with FIFO enabled(EDMA path)
*************************************************************************/
/* CSL specific include files */
#include <csl.h>
#include <csl_edma3.h>
#include <csl_intc.h>
#include <csl_edma3Aux.h>
#include <cslr_device.h>
#include <cslr_mcbsp.h>
#include <csl_mcbsp.h>
#include <val_util.h> /* Common utility specific */
/** Header files corresponding to MCBSP module*/
#include <mcbsp_common.h> /* McBSP common functions */
#include <edma_mcbsp_common.h> /* EDMA common functions */
//#include <mcbsp_intr.h> /* McBSP and EDMA Interrupt Setup and ISRs*/
#include <test_init.h> /* Testcase specific */
#include <csl_mcbspAux.h>
#include <fifo.h>
#include <event_defines.h>
#include <stdio.h>
#include <ti/csl/csl_cache.h>
#include <ti/csl/csl_cacheAux.h>
#define CLKGDV_START_VALUE 0
#pragma DATA_SECTION(xmtBuff0, ".Xmt_data") /* xmtBuff can be in L2, DDR or MSMC.Here it is in L2 */
Uint32 xmtBuff0[NUM_XMT_ELEMENTS];
#pragma DATA_SECTION(xmtBuff1,".Xmt_data")
Uint32 xmtBuff1[NUM_XMT_ELEMENTS];
#pragma DATA_SECTION(rcvBuff0, ".Rcv_data") /* rcvBuff can be in L2, DDR or MSMC.Here it is in L2 */
Uint32 rcvBuff0[NUM_RCV_ELEMENTS];
#pragma DATA_SECTION(rcvBuff1, ".Rcv_data")
Uint32 rcvBuff1[NUM_RCV_ELEMENTS];
#pragma DATA_SECTION(profile_results, ".msmcData")
Uint32 profile_results[500];
Uint32 MCBSP0_BASE_ADDRESS;
//Uint32 profile_results[];
Uint32 *profileresultsPtr;
CSL_Status status; /* CSL status variable */
CSL_McbspIntMode mytxInt,myrxInt; /* interrupt scratchpad variables */
CSL_BitMask32 secEventLo = -1;
CSL_BitMask32 secEventHi = -1;
CSL_BitMask32 missedLo = -1;
CSL_BitMask32 missedHi = -1;
CSL_BitMask32 missedQdma = -1;
extern fifo_info myfifo;
Uint32 main(void)
{
Uint32 failFlag = 0;
Uint32 mcbspError = 0;
Uint32 intrEn[2] = {0,0};
Uint32 i = 0, j, k;
Uint32 mcbsp1_spcr = 0, mcbsp0_spcr = 0;
Uint32 edma_done = 0, sync_error = 0;
Uint32 result;
Uint32 err_val = 0;
Uint32 no_of_elements;
//Uint32 no_of_receive_elements;
Uint32 MCBSP0_BASE_ADDRESS, MCBSP1_BASE_ADDRESS;
volatile Uint32 * writeAddress0;
volatile Uint32 * writeAddress1;
volatile Uint32 * readAddress0;
volatile Uint32 * readAddress1;
Uint32 * xmtBuff0_global;
Uint32 * rcvBuff0_global;
Uint32 * xmtBuff1_global;
Uint32 * rcvBuff1_global;
Uint32 temp_TCC_Tx[2];
Uint32 temp_TCC_Rx[2];
CSL_Edma3CmdIntr ipr;
Uint32 Mcbsp0_Tx_Edma_Done = 0;
Uint32 Mcbsp0_Rcv_Edma_Done = 0;
Uint32 Mcbsp1_Tx_Edma_Done = 0;
Uint32 Mcbsp1_Rcv_Edma_Done = 0;
Uint32 Xfr_Complete_Code_Mcbsp_Tx[2] = {CSL_EDMACC_2_CHA_XEVT0,CSL_EDMACC_2_CHA_XEVT1};
Uint32 Xfr_Complete_Code_Mcbsp_Rx[2] = {CSL_EDMACC_2_CHA_REVT0,CSL_EDMACC_2_CHA_REVT1};
Uint32 acnt, bcnt,srcBIDX,dstBIDX;
//Since internal clock coming to Mcbsp is CPU/6=166.67MHz,max freq upto which we can check is 83.34MHz
Uint32 Mcbsp_Div[MAX_ITERATIONS]={0x3,0x2,0x1,0x0};
//disable L1D/L2 cache
CACHE_setL1DSize(CACHE_L1_0KCACHE);
CACHE_setL2Size(CACHE_0KCACHE);
VAL_TRACE(0xAAAA0000);
profileresultsPtr = (Uint32 *)profile_results; /* Assign Results array to the pointer */
/* for loop for the various iterations...In 1st iteration FIFO is disabled..In 2nd iteration
FIFO is enabled but with WNUM_EVT/RNUM_EVT =1 word..i.e there is no effect of FIFO usage..
In the following iterations WNUM_EVT/RNUM_EVT value is gradually increased in multiples of 8
i.e. 8,16, 24..upto 64 words which is the max*/
EDMA3_ModuleInitOpen(); /* Initialize the EDMA Module and open a handle */
CSL_mcbspInit(0); /* Initialize the MCBSP CSL */
for(j=0;j<NUM_OF_ITERATIONS;j++)
{
failFlag = 0;
VAL_TRACE(0xAAAA0002);
/*Initialise all the Mcbsp and EDMA handles to NULL */
hMcbsp0ChTx = NULL; hMcbsp0ChRx = NULL; hParamMcbsp0Tx = NULL; hParamMcbsp0Rx = NULL;
hMcbsp1ChTx = NULL; hMcbsp1ChRx = NULL; hParamMcbsp1Tx = NULL; hParamMcbsp1Rx = NULL;
/*Open, Reset and Configure the McBSP Handle */
hMcbsp[0] = CSL_mcbspOpen(&myMcbspObj[0],
CSL_MCBSP_PERI[0],
NULL,
&status);
hMcbsp[1] = CSL_mcbspOpen(&myMcbspObj[1],
CSL_MCBSP_PERI[1],
NULL,
&status);
/*Open the EMDA Handles for McBSP0 and McBSP1 Channels*/
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_A, EDMA_MCBSP_CHA_TX_DIR, &hMcbsp0ChTx);
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_A, EDMA_MCBSP_CHA_RX_DIR, &hMcbsp0ChRx);
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_B, EDMA_MCBSP_CHA_TX_DIR, &hMcbsp1ChTx);
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_B, EDMA_MCBSP_CHA_RX_DIR, &hMcbsp1ChRx);
/* Initialize Data for TX and corrupt RX buffer */
Fill_McBSP_DataBuffer_Multichannel((Uint8 *)xmtBuff0,(Uint8 *) rcvBuff0, NUM_XMT_ELEMENTS);
Fill_McBSP_DataBuffer_Multichannel((Uint8 *)xmtBuff1, (Uint8 *)rcvBuff1, NUM_XMT_ELEMENTS);
/*Since there is only DXR or DRR register to write/read WNUMDMA/RNUMDMA =1 */
// no_of_xmt_elements = 128;
// no_of_receive_elements = 128;
switch(j)
{
case(0):
{
myfifo.WriteFifoEnable = 0;
myfifo.ReadFifoEnable = 0;
no_of_elements = 512; //total no. of bytes of transfer
acnt = 4;
bcnt = (no_of_elements/acnt);
srcBIDX = acnt;
dstBIDX = 0;
break;
}
case(1):
{
myfifo.WriteFifoEnable = 1;
myfifo.ReadFifoEnable = 1;
myfifo.TEST_WNUMEVT = 32;
myfifo.TEST_RNUMEVT = 32;
myfifo.TEST_WNUMDMA = 1;
myfifo.TEST_RNUMDMA = 1;
no_of_elements = 512; //total no. of bytes of transfer
acnt = (myfifo.TEST_WNUMEVT *4);
bcnt = no_of_elements/acnt;
srcBIDX = acnt;
dstBIDX = acnt;
break;
}
default:
break;
}
if(myfifo.WriteFifoEnable ==1 || myfifo.ReadFifoEnable ==1)
{
MCBSP0_BASE_ADDRESS= 0x22000000;
MCBSP1_BASE_ADDRESS= 0x22400000;
writeAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000004); //DXR offset for the DMA path is 0x04
readAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000000); //DRR offset for the DMA path is 0x00
writeAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000004);
readAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000000);
}
else
{
MCBSP0_BASE_ADDRESS= 0x021B4000;
MCBSP1_BASE_ADDRESS= 0x021B8000;
writeAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000004); //DXR offset for the CPU path is 0x04
readAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000000); //DRR offset for the CPU path is 0x00
writeAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000004);
readAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000000);
}
/* Enable the events on the EDMA*/
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Tx[0]));
CSL_edma3HwChannelControl(hMcbsp0ChTx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Rx[0]));
CSL_edma3HwChannelControl(hMcbsp0ChRx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Tx[1]));
CSL_edma3HwChannelControl(hMcbsp1ChTx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Rx[1]));
CSL_edma3HwChannelControl(hMcbsp1ChRx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
temp_TCC_Tx[0] = (Xfr_Complete_Code_Mcbsp_Tx[0]-32);
temp_TCC_Tx[1] = (Xfr_Complete_Code_Mcbsp_Tx[1]-32);
temp_TCC_Rx[0] = (Xfr_Complete_Code_Mcbsp_Rx[0]-32);
temp_TCC_Rx[1] = (Xfr_Complete_Code_Mcbsp_Rx[1]-32);
ipr.region=CSL_EDMA3_REGION_GLOBAL;
ipr.intrh= (1 << temp_TCC_Tx[0])\
|(1 << temp_TCC_Tx[1])\
|(1 << temp_TCC_Rx[0])\
|(1 << temp_TCC_Rx[1]);
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,&ipr);
xmtBuff0_global = (Uint32 *) global_address((Uint32)xmtBuff0);
rcvBuff0_global = (Uint32 *) global_address((Uint32)rcvBuff0);
xmtBuff1_global = (Uint32 *) global_address((Uint32)xmtBuff1);
rcvBuff1_global = (Uint32 *) global_address((Uint32)rcvBuff1);
// Wait for interrupt
ipr.region = CSL_EDMA3_REGION_GLOBAL;
ipr.intr = 0;
ipr.intrh = 0;
/* Iteration number varies from 0 to CLKGDV_START_VALUE */
for(i = 0; i <MAX_ITERATIONS; i++)
{
VAL_TRACE(0xcace1100 + i);
/* Reset the MCBSP Channel */
CSL_mcbspHwControl (hMcbsp[0], CSL_MCBSP_CMD_RESET, 0);
CSL_mcbspHwControl (hMcbsp[1], CSL_MCBSP_CMD_RESET, 0);
/* configure for 128 channel mode*/
Configure_MultiChannel(CSL_MCBSP_A, xmt_channels, rcv_channels);
Configure_MultiChannel(CSL_MCBSP_B, xmt_channels, rcv_channels);
MCBSP_HwSetupStructFill(Mcbsp_Div[i]); /* Populate the McBSP parameters into local structure */
/* Fill RX buffer for both the McBSP's with zeroes */
Corrupt_McBSP_DataBuffer(rcvBuff0, NUM_RCV_ELEMENTS);
Corrupt_McBSP_DataBuffer(rcvBuff1, NUM_RCV_ELEMENTS);
CSL_mcbspHwSetup(hMcbsp[0], &mySetup); /* Configure the Mcbsp registers */
CSL_mcbspHwSetup(hMcbsp[1], &mySetup);
Edma_Mcbsp_Setup (CSL_MCBSP_A, /* Setup the EMDA for McBSP0 */
readAddress0,
writeAddress0,
&hMcbsp0ChTx,
&hMcbsp0ChRx,
&hParamMcbsp0Tx,
&hParamMcbsp0Rx,
xmtBuff0_global,
rcvBuff0_global,
Xfr_Complete_Code_Mcbsp_Tx[0],
Xfr_Complete_Code_Mcbsp_Rx[0],
acnt,
bcnt,
srcBIDX,
dstBIDX);
Edma_Mcbsp_Setup (CSL_MCBSP_B, /* Setup the EMDA for McBSP1 */
readAddress1,
writeAddress1,
&hMcbsp1ChTx,
&hMcbsp1ChRx,
&hParamMcbsp1Tx,
&hParamMcbsp1Rx,
xmtBuff1_global,
rcvBuff1_global,
Xfr_Complete_Code_Mcbsp_Tx[1],
Xfr_Complete_Code_Mcbsp_Rx[1],
acnt,
bcnt,
srcBIDX,
dstBIDX);
/*Initialize the FIFO*/
InitBfifo_0(myfifo.TEST_WNUMDMA, myfifo.TEST_WNUMEVT, myfifo.TEST_RNUMDMA, myfifo.TEST_RNUMEVT);
InitBfifo_1(myfifo.TEST_WNUMDMA, myfifo.TEST_WNUMEVT, myfifo.TEST_RNUMDMA, myfifo.TEST_RNUMEVT);
VAL_TRACE(0x98989898);
for(k=0; k <= 50; k++); //adding delay
Tx_Rx_Clkgen_Frmgen(hMcbsp[0], MCBSP_ENABLE); /*Enable TX, RX, SRGR clock and SRGR Frame generation */
Tx_Rx_Clkgen_Frmgen(hMcbsp[1], MCBSP_ENABLE);
VAL_TRACE(0x99990000);
do
{
CSL_edma3GetHwStatus(hModule,
CSL_EDMA3_QUERY_INTRPEND,
&ipr);
}while(ipr.intrh!= 0x000000F0);
if(ipr.intrh & (1 << temp_TCC_Tx[0]))
{
Mcbsp0_Tx_Edma_Done = 1;
VAL_TRACE(0xedcb0000 + temp_TCC_Tx[0]);
}
if(ipr.intrh & (1 << temp_TCC_Tx[1]))
{
Mcbsp1_Tx_Edma_Done = 1;
VAL_TRACE(0xedcb1000 + temp_TCC_Tx[1]);
}
if(ipr.intrh & (1 << temp_TCC_Rx[0]))
{
Mcbsp0_Rcv_Edma_Done = 1;
VAL_TRACE(0xedcb0100 + temp_TCC_Rx[0]);
}
if(ipr.intrh & (1 << temp_TCC_Rx[1]))
{
Mcbsp1_Rcv_Edma_Done = 1;
VAL_TRACE(0xedcb1100 + temp_TCC_Rx[1]);
}
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,&ipr);
// }while(ipr.intrh!= 0);
/* Set Interrupt EVAL */
ipr.intr = 0x00000000;
ipr.intrh = 0x00000000;
edma_done = Mcbsp0_Tx_Edma_Done + Mcbsp0_Rcv_Edma_Done + Mcbsp1_Tx_Edma_Done + Mcbsp1_Rcv_Edma_Done;
/* Disable TX, RX, SRGR clock and SRGR Frame generation */
Tx_Rx_Clkgen_Frmgen(hMcbsp[0], MCBSP_DISABLE);
Tx_Rx_Clkgen_Frmgen(hMcbsp[1], MCBSP_DISABLE);
VAL_TRACE(0xeeee0000 + mcbspError);
failFlag =0;
/* Data comparison for McBSP0 and McBSP1 */
//// if(mcbspError == 0)
// {
failFlag = Compare_McBSP_DataBuffer_MultiChannel(xmtBuff0,
rcvBuff0,
NUM_XFR_ITERATIONS,
FRAME_LENGTH1,
xmt_channels,
rcv_channels,
mytxdata.wordLength1,
mytxdata.rjust_dxenable);
failFlag = (failFlag & (Compare_McBSP_DataBuffer_MultiChannel(xmtBuff1,
rcvBuff1,
NUM_XFR_ITERATIONS,
FRAME_LENGTH1,
xmt_channels,
rcv_channels,
mytxdata.wordLength1,
mytxdata.rjust_dxenable)));
VAL_TRACE(0xAAAAABCD);
if (failFlag != PASS)
{
VAL_TRACE(0xDEAD0000 + i);
VAL_TRACE(mcbsp0_spcr);
VAL_TRACE(mcbsp1_spcr);
*(profileresultsPtr++) = i; //Store iteration number i
*(profileresultsPtr++) = j;
VAL_TRACE(myclkset.srgClkDivide);
*(profileresultsPtr++) = Mcbsp_Div[i]; //Store corresponding CLKGDV value
*(profileresultsPtr++) = 0xDEADDEAD;
result = FAIL;
}
else
{
VAL_TRACE(0xABCDABCD);
*(profileresultsPtr++) = i; //Store iteration number i
*(profileresultsPtr++) = j;
VAL_TRACE(myclkset.srgClkDivide);
*(profileresultsPtr++) = Mcbsp_Div[i]; //Store corresponding CLKGDV value
*(profileresultsPtr++) = 0xABCDABCD;
result = PASS;
}
/* Clear SEC bits corresponding to EDMA Channel numbers used by writing into SECR register.
This is to be repeated for every iteration */
CSL_edma3ClearDMASecondaryEvents(hModule,secEventLo,secEventHi);
CSL_edma3EventsMissedClear(hModule,missedLo, missedHi, missedQdma);
Mcbsp0_Tx_Edma_Done = 0; Mcbsp0_Rcv_Edma_Done = 0;
Mcbsp1_Tx_Edma_Done = 0; Mcbsp1_Rcv_Edma_Done = 0;
// rxd_cnt0 = 0; txd_cnt0 = 0; rxd_cnt1 = 0; txd_cnt1 = 0;
edma_done = 0; sync_error = 0;
} // end... for(i = 0; (i <= (CLKGDV_START_VALUE - 1)) && (mcbspError == 0); i++)
}
/* Close the EDMA channel opened for McBSP Transmit and Recieve */
EDMA_Mcbsp_ChannelClose(&hMcbsp0ChTx, &hMcbsp0ChRx);
EDMA_Mcbsp_ChannelClose(&hMcbsp1ChTx, &hMcbsp1ChRx);
status = CSL_mcbspClose(hMcbsp[0]); /* Close the McBSP Handle*/
status = CSL_mcbspClose(hMcbsp[1]);
CSL_edma3Close(hModule); /* Close the EDMA Module*/
if (result == PASS)
printf("Test passed\n");
else
printf("Test failed\n");
return(result);
}
void MCBSP_HwSetupStructFill(Uint32 ClkDiv)
{
/*************************************************************************/
/* \brief Configure the MCBSP with following values.
*************************************************************************
** \note McBSP receiver, transmitter frame sync logic and sample rate
** generator are not enabled in this function. This is done because
** once these are enabled, McBSP will start its operation, which might
** not be required till DMA and IRQ setups, if any are done.
*************************************************************************/
myglobal.ioEnableMode = CSL_MCBSP_IOMODE_TXDIS_RXDIS;
#ifdef TB_LOOPBACK
myglobal.dlbMode = CSL_MCBSP_DLBMODE_OFF;
#else
myglobal.dlbMode = CSL_MCBSP_DLBMODE_ON; // DLB mode
#endif
myglobal.clkStopMode = CSL_MCBSP_CLKSTP_DISABLE;
myrxdata.wordReverse = CSL_MCBSP_32BIT_REVERS_DISABLE;
myrxdata.numPhases = CSL_MCBSP_PHASE_SINGLE;
myrxdata.wordLength1 = CSL_MCBSP_WORDLEN_32;
myrxdata.frmLength1 = FRAME_LENGTH1;
myrxdata.wordLength2 = CSL_MCBSP_WORDLEN_8;
myrxdata.frmLength2 = FRAME_LENGTH2;
myrxdata.frmSyncIgn = CSL_MCBSP_FRMSYNC_DETECT;
myrxdata.compand = CSL_MCBSP_COMPAND_OFF_MSB_FIRST;
myrxdata.dataDelay = CSL_MCBSP_DATADELAY_0_BIT;
myrxdata.rjust_dxenable = CSL_MCBSP_RJUSTDXENA_RJUST_RZF;
myrxdata.intEvent = CSL_MCBSP_INTMODE_ON_SYNCERR; // RINTM of SPCR . Value is 2'b11
mytxdata.wordReverse = CSL_MCBSP_32BIT_REVERS_DISABLE;
mytxdata.numPhases = CSL_MCBSP_PHASE_SINGLE;
mytxdata.wordLength1 = CSL_MCBSP_WORDLEN_32;
mytxdata.frmLength1 = FRAME_LENGTH1;
mytxdata.wordLength2 = CSL_MCBSP_WORDLEN_8;
mytxdata.frmLength2 = FRAME_LENGTH2;
mytxdata.frmSyncIgn = CSL_MCBSP_FRMSYNC_DETECT;
mytxdata.compand = CSL_MCBSP_COMPAND_OFF_MSB_FIRST;
mytxdata.dataDelay = CSL_MCBSP_DATADELAY_0_BIT;
mytxdata.rjust_dxenable = CSL_MCBSP_RJUSTDXENA_RJUST_RZF;
mytxdata.intEvent = CSL_MCBSP_INTMODE_ON_FSYNC; //XINTM OF SPCR.Value is 2'b10
myclkset.frmSyncTxMode = CSL_MCBSP_FSCLKMODE_INTERNAL; // Refers to FSXM field of PCR register
myclkset.frmSyncRxMode = CSL_MCBSP_FSCLKMODE_EXTERNAL; // Refers to FSRM field of PCR register
// myclkset.frmSyncRxMode = CSL_MCBSP_FSCLKMODE_INTERNAL;
myclkset.clkRxMode = CSL_MCBSP_TXRXCLKMODE_EXTERNAL; // Refers to CLKRM field of PCR register
myclkset.clkTxMode = CSL_MCBSP_TXRXCLKMODE_INTERNAL; // Refers to CLKXM field of PCR register
myclkset.frmSyncTxPolarity = CSL_MCBSP_FSPOL_ACTIVE_LOW; //Refers to FSXP field of PCR register
myclkset.frmSyncRxPolarity = CSL_MCBSP_FSPOL_ACTIVE_LOW; //Refers to FSRP field of PCR register
myclkset.clkTxPolarity = CSL_MCBSP_CLKPOL_TX_FALLING_EDGE; //Refers to CLKXP field of PCR register
myclkset.clkRxPolarity = CSL_MCBSP_CLKPOL_RX_RISING_EDGE; //Refers to CLKRP field of PCR register
myclkset.srgClkDivide = ClkDiv ; //CLKGDIV OF SRGR
myclkset.srgFrmPulseWidth = FRAME_PULSE_WIDTH; //FWID OF SRGR
myclkset.srgFrmPeriod = FRAME_PERIOD; //FPER OF SRGR
//myclkset.srgInputClkMode = CSL_MCBSP_SRGCLK_CLKS; //CLKSM OF SGRGR i.e External clock source.
myclkset.srgInputClkMode = CSL_MCBSP_SRGCLK_CLKCPU; //Change from external clk to CPU clock
myclkset.srgClkPolarity = CSL_MCBSP_CLKPOL_SRG_RISING_EDGE; //CLKSP OF SRGR
myclkset.srgTxFrmSyncMode = CSL_MCBSP_TXFSMODE_SRG; // FSGM OF SRGR
myclkset.srgClkSync = CSL_MCBSP_CLKGSYNCMODE_OFF; //GSYNC OF SRGR
mymulCh.rxPartition = CSL_MCBSP_PARTMODE_8PARTITION; //All 128 Channels are enabled
mymulCh.txPartition = CSL_MCBSP_PARTMODE_8PARTITION;
mymulCh.rxMulChSel = CSL_MCBSP_MULTI_CHANNEL_RX_EN_ALL; // RMCM =0 in MCR register
mymulCh.txMulChSel = CSL_MCBSP_MULTI_CHANNEL_TX_EN_NO_MASK; //XMCM =2'b01 in MCR reg
mymulCh.rxPartABlk = CSL_MCBSP_PABLK_0;
mymulCh.rxPartBBlk = CSL_MCBSP_PBBLK_1;
mymulCh.txPartABlk = CSL_MCBSP_PABLK_0;
mymulCh.txPartBBlk = CSL_MCBSP_PBBLK_1;
//mySetup.emumode = CSL_MCBSP_EMU_STOP;
mySetup.emumode = CSL_MCBSP_EMU_FREERUN;
mySetup.global = &myglobal;
mySetup.rxdataset = &myrxdata;
mySetup.txdataset = &mytxdata;
mySetup.clkset = &myclkset;
mySetup.mulCh = &mymulCh;
}
This code is not halting now. But the result is fail. I need to debug. The buffers looks like fine. However the result is fail. I shall try some more.
What needs to be done to make this ping-pong continuous (infinite). And read proper buffer (ping/pong buffers).
Thanks,
Hari
Upto rcvBuff[0x008c0120] the values match with TxBuf.
From rcvBuff[0x008c0120] to rcvBuff[0x008c0140] all values are ZEROS.
Then again there is a match from 0x008c0140 to 0x008c01a0
Again there are some zeros. Again it matches. So in between it writes ZEROS.
The total is 128 * 4 bytes = 0x200 locations. It has done one transfer.
Hi Steven,
I make all the changes that you suggested. and it still hang in the loop with ipr.intrh = 0x000000E0. It is no longer 0x000000A0, but still is not 0x000000F0.
do
{
CSL_edma3GetHwStatus(hModule, CSL_EDMA3_QUERY_INTRPEND, &ipr);
} while(ipr.intrh!= 0x000000F0);
Here is my main.c
/*****************************************************************************\
* TEXAS INSTRUMENTS INCORPORATED PROPRIETARY INFORMATION
*
* Property of Texas Instruments
* For Unrestricted Internal Use Only
* Unauthorized reproduction and/or distribution is strictly prohibited.
* This product is protected under copyright law and trade secret law
* as an unpublished work.
* Created 2011, (C) Copyright 2008 Texas Instruments. All rights reserved.
*------------------------------------------------------------------------------
* Filename : tput_search_128ch_32bit.c
* Date Created : July 21, 2011
* Last Modified :
* Description : Checks the throughput of McBSP by running the testcase at
* different clock frequencies and records first frequency
* the test case fails. McBSP transfer requests are routed
* through Config bus.
* History : Ported from CURIE
* Project : Gauss
* Author : Kanchana
\*****************************************************************************/
/* ** \Register Configurations:
** -# No Of Phase - 1,
** -# Word Length - 32,
** -# Frame Length - 128,
** -# Data Delay - 0,
** -# Interrupt on Mcbsp Transmitter and Receiver SYNC Error conditions.
EDMA Interrupts for Event Completion.
** -# XCLK --> RCLK, Internal XFS --> RFS
** -# Loop Back Mode - DLB ON,
** -# Internal Frame Sync Generation from Sample Rate Generator
** -# Frame Sync Pulse Width - 1,
** -# Frame Sync Period - 0xFFF for 128 Channels,
** -# Clock Divide Value - Variable,
** -# Enhanced Multi channel selection Enable (128 Channels)
** -#First run with FIFO disabled(CFG path), then with FIFO enabled(EDMA path)
*************************************************************************/
/* CSL specific include files */
#include <csl.h>
#include <csl_edma3.h>
#include <csl_intc.h>
#include <csl_edma3Aux.h>
#include <cslr_device.h>
#include <cslr_mcbsp.h>
#include <csl_mcbsp.h>
#include <val_util.h> /* Common utility specific */
/** Header files corresponding to MCBSP module*/
#include <mcbsp_common.h> /* McBSP common functions */
#include <edma_mcbsp_common.h> /* EDMA common functions */
//#include <mcbsp_intr.h> /* McBSP and EDMA Interrupt Setup and ISRs*/
#include <test_init.h> /* Testcase specific */
#include <csl_mcbspAux.h>
#include <fifo.h>
#include <event_defines.h>
#include <stdio.h>
#include <ti/csl/csl_cache.h>
#include <ti/csl/csl_cacheAux.h>
// SQ #define CLKGDV_START_VALUE 0
//Uint16 xmt_channels[] = {0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF};
//Uint16 rcv_channels[] = {0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF,0xFFFF};
Uint16 xmt_channels[] = {0xFFFF,0xFFFF,0,0,0,0,0,0};
Uint16 rcv_channels[] = {0xFFFF,0xFFFF,0,0,0,0,0,0};
#pragma DATA_SECTION(xmtBuff0, ".Xmt_data") /* xmtBuff can be in L2, DDR or MSMC.Here it is in L2 */
Uint32 xmtBuff0[NUM_XMT_ELEMENTS];
#pragma DATA_SECTION(xmtBuff1,".Xmt_data")
Uint32 xmtBuff1[NUM_XMT_ELEMENTS];
#pragma DATA_SECTION(rcvBuff0, ".Rcv_data") /* rcvBuff can be in L2, DDR or MSMC.Here it is in L2 */
Uint32 rcvBuff0[NUM_RCV_ELEMENTS];
#pragma DATA_SECTION(rcvBuff1, ".Rcv_data")
Uint32 rcvBuff1[NUM_RCV_ELEMENTS];
#pragma DATA_SECTION(profile_results, ".msmcData")
Uint32 profile_results[500];
Uint32 MCBSP0_BASE_ADDRESS;
//Uint32 profile_results[];
Uint32 *profileresultsPtr;
CSL_Status status; /* CSL status variable */
CSL_McbspIntMode mytxInt,myrxInt; /* interrupt scratchpad variables */
CSL_BitMask32 secEventLo = 0xFFFFFFFF;
CSL_BitMask32 secEventHi = 0xFFFFFFFF;
CSL_BitMask32 missedLo = 0xFFFFFFFF;
CSL_BitMask32 missedHi = 0xFFFFFFFF;
CSL_BitMask32 missedQdma = 0xFFFFFFFF;
extern fifo_info myfifo;
void FPGA_main(void);
/******************************************************************************/
Uint32 old_main(void);
Uint32 main(void)
{
FPGA_main();
while (1)
old_main();
}
/******************************************************************************/
Uint32 old_main(void)
{
Uint32 failFlag = 0;
Uint32 mcbspError = 0;
Uint32 intrEn[2] = {0,0};
Uint32 i = 0, j, k;
Uint32 mcbsp1_spcr = 0, mcbsp0_spcr = 0;
Uint32 edma_done = 0, sync_error = 0;
Uint32 result;
Uint32 err_val = 0;
Uint32 no_of_elements;
//Uint32 no_of_receive_elements;
Uint32 MCBSP0_BASE_ADDRESS, MCBSP1_BASE_ADDRESS;
volatile Uint32 * writeAddress0;
volatile Uint32 * writeAddress1;
volatile Uint32 * readAddress0;
volatile Uint32 * readAddress1;
Uint32 * xmtBuff0_global;
Uint32 * rcvBuff0_global;
Uint32 * xmtBuff1_global;
Uint32 * rcvBuff1_global;
Uint32 temp_TCC_Tx[2];
Uint32 temp_TCC_Rx[2];
CSL_Edma3CmdIntr ipr;
Uint32 Mcbsp0_Tx_Edma_Done = 0;
Uint32 Mcbsp0_Rcv_Edma_Done = 0;
Uint32 Mcbsp1_Tx_Edma_Done = 0;
Uint32 Mcbsp1_Rcv_Edma_Done = 0;
Uint32 Xfr_Complete_Code_Mcbsp_Tx[2] = {CSL_EDMACC_2_CHA_XEVT0,CSL_EDMACC_2_CHA_XEVT1};
Uint32 Xfr_Complete_Code_Mcbsp_Rx[2] = {CSL_EDMACC_2_CHA_REVT0,CSL_EDMACC_2_CHA_REVT1};
Uint32 acnt, bcnt,srcBIDX,dstBIDX;
//Since internal clock coming to Mcbsp is CPU/6=166.67MHz,max freq upto which we can check is 83.34MHz
Uint32 Mcbsp_Div[MAX_ITERATIONS]={0x3,0x2,0x1,0x1};
// Uint32 Mcbsp_Div[MAX_ITERATIONS]={0x1,0x1,0x1,0x1};
//disable L1D/L2 cache
CACHE_setL1DSize(CACHE_L1_0KCACHE);
CACHE_setL2Size(CACHE_0KCACHE);
VAL_TRACE(0xAAAA0000);
profileresultsPtr = (Uint32 *)profile_results; /* Assign Results array to the pointer */
/* for loop for the various iterations...In 1st iteration FIFO is disabled..In 2nd iteration
FIFO is enabled but with WNUM_EVT/RNUM_EVT =1 word..i.e there is no effect of FIFO usage..
In the following iterations WNUM_EVT/RNUM_EVT value is gradually increased in multiples of 8
i.e. 8,16, 24..upto 64 words which is the max*/
EDMA3_ModuleInitOpen(); /* Initialize the EDMA Module and open a handle */
CSL_mcbspInit(0); /* Initialize the MCBSP CSL */
// for(j=0;j<NUM_OF_ITERATIONS;j++)
for(j = 1; j < NUM_OF_ITERATIONS; j++)
{
failFlag = 0;
VAL_TRACE(0xAAAA0002);
/*Initialise all the Mcbsp and EDMA handles to NULL */
hMcbsp0ChTx = NULL; hMcbsp0ChRx = NULL; hParamMcbsp0Tx = NULL; hParamMcbsp0Rx = NULL;
hMcbsp1ChTx = NULL; hMcbsp1ChRx = NULL; hParamMcbsp1Tx = NULL; hParamMcbsp1Rx = NULL;
/*Open, Reset and Configure the McBSP Handle */
hMcbsp[0] = CSL_mcbspOpen(&myMcbspObj[0],
CSL_MCBSP_PERI[0],
NULL,
&status);
hMcbsp[1] = CSL_mcbspOpen(&myMcbspObj[1],
CSL_MCBSP_PERI[1],
NULL,
&status);
/*Open the EMDA Handles for McBSP0 and McBSP1 Channels*/
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_A, EDMA_MCBSP_CHA_TX_DIR, &hMcbsp0ChTx);
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_A, EDMA_MCBSP_CHA_RX_DIR, &hMcbsp0ChRx);
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_B, EDMA_MCBSP_CHA_TX_DIR, &hMcbsp1ChTx);
EDMA_Mcbsp_ChannelOpen(CSL_MCBSP_B, EDMA_MCBSP_CHA_RX_DIR, &hMcbsp1ChRx);
/* Initialize Data for TX and corrupt RX buffer */
Fill_McBSP_DataBuffer_Multichannel((Uint8 *)xmtBuff0,(Uint8 *)rcvBuff0, 4*NUM_XMT_ELEMENTS);
Fill_McBSP_DataBuffer_Multichannel((Uint8 *)xmtBuff1,(Uint8 *)rcvBuff1, 4*NUM_XMT_ELEMENTS);
/*Since there is only DXR or DRR register to write/read WNUMDMA/RNUMDMA =1 */
// no_of_xmt_elements = 128;
// no_of_receive_elements = 128;
switch(j)
{
case(0):
{
myfifo.WriteFifoEnable = 0;
myfifo.ReadFifoEnable = 0;
no_of_elements = 512; //total no. of bytes of transfer
acnt = 4;
bcnt = (no_of_elements/acnt);
srcBIDX = acnt;
dstBIDX = 0;
break;
}
case(1):
{
myfifo.WriteFifoEnable = 1;
myfifo.ReadFifoEnable = 1;
myfifo.TEST_WNUMEVT = 32;
myfifo.TEST_RNUMEVT = 32;
myfifo.TEST_WNUMDMA = 1;
myfifo.TEST_RNUMDMA = 1;
no_of_elements = 512; //total no. of bytes of transfer
acnt = (myfifo.TEST_WNUMEVT *4);
bcnt = no_of_elements/acnt;
srcBIDX = acnt;
dstBIDX = acnt;
break;
}
default:
break;
}
if(myfifo.WriteFifoEnable ==1 || myfifo.ReadFifoEnable ==1)
{
MCBSP0_BASE_ADDRESS= 0x22000000;
MCBSP1_BASE_ADDRESS= 0x22400000;
writeAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000004); //DXR offset for the DMA path is 0x04
readAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000000); //DRR offset for the DMA path is 0x00
writeAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000004);
readAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000000);
}
else
{
MCBSP0_BASE_ADDRESS= 0x021B4000;
MCBSP1_BASE_ADDRESS= 0x021B8000;
writeAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000004); //DXR offset for the CPU path is 0x04
readAddress0 = (Uint32 *)(MCBSP0_BASE_ADDRESS + 0x00000000); //DRR offset for the CPU path is 0x00
writeAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000004);
readAddress1 = (Uint32 *)(MCBSP1_BASE_ADDRESS + 0x00000000);
}
/* Enable the events on the EDMA*/
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Tx[0]));
CSL_edma3HwChannelControl(hMcbsp0ChTx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Rx[0]));
CSL_edma3HwChannelControl(hMcbsp0ChRx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Tx[1]));
CSL_edma3HwChannelControl(hMcbsp1ChTx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
intrEn[0] = (1 << (Xfr_Complete_Code_Mcbsp_Rx[1]));
CSL_edma3HwChannelControl(hMcbsp1ChRx, CSL_EDMA3_CMD_CHANNEL_ENABLE, intrEn);
temp_TCC_Tx[0] = (Xfr_Complete_Code_Mcbsp_Tx[0]-32);
temp_TCC_Tx[1] = (Xfr_Complete_Code_Mcbsp_Tx[1]-32);
temp_TCC_Rx[0] = (Xfr_Complete_Code_Mcbsp_Rx[0]-32);
temp_TCC_Rx[1] = (Xfr_Complete_Code_Mcbsp_Rx[1]-32);
ipr.region= CSL_EDMA3_REGION_GLOBAL;
ipr.intrh = (1 << temp_TCC_Tx[0])|(1 << temp_TCC_Tx[1])|
(1 << temp_TCC_Rx[0])|(1 << temp_TCC_Rx[1]);
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,&ipr);
xmtBuff0_global = (Uint32 *) global_address((Uint32)xmtBuff0);
rcvBuff0_global = (Uint32 *) global_address((Uint32)rcvBuff0);
xmtBuff1_global = (Uint32 *) global_address((Uint32)xmtBuff1);
rcvBuff1_global = (Uint32 *) global_address((Uint32)rcvBuff1);
// Wait for interrupt
ipr.region = CSL_EDMA3_REGION_GLOBAL;
ipr.intr = 0;
ipr.intrh = 0;
/* Iteration number varies from 0 to CLKGDV_START_VALUE */
// for(i = 0; i <MAX_ITERATIONS; i++)
for(i = 3; i <MAX_ITERATIONS; i++)
{
VAL_TRACE(0xcace1100 + i);
/* Reset the MCBSP Channel */
CSL_mcbspHwControl (hMcbsp[0], CSL_MCBSP_CMD_RESET, 0);
CSL_mcbspHwControl (hMcbsp[1], CSL_MCBSP_CMD_RESET, 0);
/* configure for 128 channel mode*/
Configure_MultiChannel(CSL_MCBSP_A, xmt_channels, rcv_channels);
Configure_MultiChannel(CSL_MCBSP_B, xmt_channels, rcv_channels);
MCBSP_HwSetupStructFill(Mcbsp_Div[i]); /* Populate the McBSP parameters into local structure */
/* Fill RX buffer for both the McBSP's with zeroes */
Corrupt_McBSP_DataBuffer(rcvBuff0, NUM_RCV_ELEMENTS);
Corrupt_McBSP_DataBuffer(rcvBuff1, NUM_RCV_ELEMENTS);
CSL_mcbspHwSetup(hMcbsp[0], &mySetup); /* Configure the Mcbsp registers */
CSL_mcbspHwSetup(hMcbsp[1], &mySetup);
// enable Frame Sync and Sample-Rate Generator.
*(int *)(0x21b4008) |= 0x00C00000;
*(int *)(0x21b8008) |= 0x00C00000;
Edma_Mcbsp_Setup (CSL_MCBSP_A, /* Setup the EMDA for McBSP0 */
readAddress0,
writeAddress0,
&hMcbsp0ChTx,
&hMcbsp0ChRx,
&hParamMcbsp0Tx,
&hParamMcbsp0Rx,
xmtBuff0_global,
rcvBuff0_global,
Xfr_Complete_Code_Mcbsp_Tx[0],
Xfr_Complete_Code_Mcbsp_Rx[0],
acnt,
bcnt,
srcBIDX,
dstBIDX);
Edma_Mcbsp_Setup (CSL_MCBSP_B, /* Setup the EMDA for McBSP1 */
readAddress1,
writeAddress1,
&hMcbsp1ChTx,
&hMcbsp1ChRx,
&hParamMcbsp1Tx,
&hParamMcbsp1Rx,
xmtBuff1_global,
rcvBuff1_global,
Xfr_Complete_Code_Mcbsp_Tx[1],
Xfr_Complete_Code_Mcbsp_Rx[1],
acnt,
bcnt,
srcBIDX,
dstBIDX);
/*Initialize the FIFO*/
InitBfifo_0(myfifo.TEST_WNUMDMA, myfifo.TEST_WNUMEVT, myfifo.TEST_RNUMDMA, myfifo.TEST_RNUMEVT);
InitBfifo_1(myfifo.TEST_WNUMDMA, myfifo.TEST_WNUMEVT, myfifo.TEST_RNUMDMA, myfifo.TEST_RNUMEVT);
VAL_TRACE(0x98989898);
for(k=0; k <= 50; k++); //adding delay
Tx_Rx_Clkgen_Frmgen(hMcbsp[0], MCBSP_ENABLE); /*Enable TX, RX, SRGR clock and SRGR Frame generation */
Tx_Rx_Clkgen_Frmgen(hMcbsp[1], MCBSP_ENABLE);
VAL_TRACE(0x99990000);
do
{
CSL_edma3GetHwStatus(hModule,
CSL_EDMA3_QUERY_INTRPEND,
&ipr);
}while(ipr.intrh!= 0x000000F0);
if(ipr.intrh & (1 << temp_TCC_Tx[0]))
{
Mcbsp0_Tx_Edma_Done = 1;
VAL_TRACE(0xedcb0000 + temp_TCC_Tx[0]);
}
if(ipr.intrh & (1 << temp_TCC_Tx[1]))
{
Mcbsp1_Tx_Edma_Done = 1;
VAL_TRACE(0xedcb1000 + temp_TCC_Tx[1]);
}
if(ipr.intrh & (1 << temp_TCC_Rx[0]))
{
Mcbsp0_Rcv_Edma_Done = 1;
VAL_TRACE(0xedcb0100 + temp_TCC_Rx[0]);
}
if(ipr.intrh & (1 << temp_TCC_Rx[1]))
{
Mcbsp1_Rcv_Edma_Done = 1;
VAL_TRACE(0xedcb1100 + temp_TCC_Rx[1]);
}
CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,&ipr);
// }while(ipr.intrh!= 0);
/* Set Interrupt EVAL */
ipr.intr = 0x00000000;
ipr.intrh = 0x00000000;
edma_done = Mcbsp0_Tx_Edma_Done + Mcbsp0_Rcv_Edma_Done + Mcbsp1_Tx_Edma_Done + Mcbsp1_Rcv_Edma_Done;
/* Disable TX, RX, SRGR clock and SRGR Frame generation */
Tx_Rx_Clkgen_Frmgen(hMcbsp[0], MCBSP_DISABLE);
Tx_Rx_Clkgen_Frmgen(hMcbsp[1], MCBSP_DISABLE);
VAL_TRACE(0xeeee0000 + mcbspError);
failFlag =0;
/* Data comparison for McBSP0 and McBSP1 */
//// if(mcbspError == 0)
// {
failFlag = Compare_McBSP_DataBuffer_MultiChannel(xmtBuff0,
rcvBuff0,
NUM_XFR_ITERATIONS,
FRAME_LENGTH1,
xmt_channels,
rcv_channels,
mytxdata.wordLength1,
mytxdata.rjust_dxenable);
failFlag = (failFlag & (Compare_McBSP_DataBuffer_MultiChannel(xmtBuff1,
rcvBuff1,
NUM_XFR_ITERATIONS,
FRAME_LENGTH1,
xmt_channels,
rcv_channels,
mytxdata.wordLength1,
mytxdata.rjust_dxenable)));
VAL_TRACE(0xAAAAABCD);
if (failFlag != PASS)
{
VAL_TRACE(0xDEAD0000 + i);
VAL_TRACE(mcbsp0_spcr);
VAL_TRACE(mcbsp1_spcr);
*(profileresultsPtr++) = i; //Store iteration number i
*(profileresultsPtr++) = j;
VAL_TRACE(myclkset.srgClkDivide);
*(profileresultsPtr++) = Mcbsp_Div[i]; //Store corresponding CLKGDV value
*(profileresultsPtr++) = 0xDEADDEAD;
result = FAIL;
}
else
{
VAL_TRACE(0xABCDABCD);
*(profileresultsPtr++) = i; //Store iteration number i
*(profileresultsPtr++) = j;
VAL_TRACE(myclkset.srgClkDivide);
*(profileresultsPtr++) = Mcbsp_Div[i]; //Store corresponding CLKGDV value
*(profileresultsPtr++) = 0xABCDABCD;
result = PASS;
}
/* Clear SEC bits corresponding to EDMA Channel numbers used by writing into SECR register.
This is to be repeated for every iteration */
CSL_edma3ClearDMASecondaryEvents(hModule,secEventLo,secEventHi);
CSL_edma3EventsMissedClear(hModule,missedLo, missedHi, missedQdma);
Mcbsp0_Tx_Edma_Done = 0; Mcbsp0_Rcv_Edma_Done = 0;
Mcbsp1_Tx_Edma_Done = 0; Mcbsp1_Rcv_Edma_Done = 0;
// rxd_cnt0 = 0; txd_cnt0 = 0; rxd_cnt1 = 0; txd_cnt1 = 0;
edma_done = 0; sync_error = 0;
} // end... for(i = 0; (i <= (CLKGDV_START_VALUE - 1)) && (mcbspError == 0); i++)
}
/* Close the EDMA channel opened for McBSP Transmit and Recieve */
EDMA_Mcbsp_ChannelClose(&hMcbsp0ChTx, &hMcbsp0ChRx);
EDMA_Mcbsp_ChannelClose(&hMcbsp1ChTx, &hMcbsp1ChRx);
status = CSL_mcbspClose(hMcbsp[0]); /* Close the McBSP Handle*/
status = CSL_mcbspClose(hMcbsp[1]);
CSL_edma3Close(hModule); /* Close the EDMA Module*/
if (result == PASS)
printf("Test passed\n");
else
printf("Test failed\n");
return(result);
}
void MCBSP_HwSetupStructFill(Uint32 ClkDiv)
{
/*************************************************************************/
/* \brief Configure the MCBSP with following values.
*************************************************************************
** \note McBSP receiver, transmitter frame sync logic and sample rate
** generator are not enabled in this function. This is done because
** once these are enabled, McBSP will start its operation, which might
** not be required till DMA and IRQ setups, if any are done.
*************************************************************************/
myglobal.ioEnableMode = CSL_MCBSP_IOMODE_TXDIS_RXDIS;
#ifdef TB_LOOPBACK
myglobal.dlbMode = CSL_MCBSP_DLBMODE_OFF;
#else
myglobal.dlbMode = CSL_MCBSP_DLBMODE_ON; // DLB mode
#endif
myglobal.clkStopMode = CSL_MCBSP_CLKSTP_DISABLE;
myrxdata.wordReverse = CSL_MCBSP_32BIT_REVERS_DISABLE;
myrxdata.numPhases = CSL_MCBSP_PHASE_SINGLE;
myrxdata.wordLength1 = CSL_MCBSP_WORDLEN_32;
myrxdata.frmLength1 = FRAME_LENGTH1;
myrxdata.wordLength2 = CSL_MCBSP_WORDLEN_8;
myrxdata.frmLength2 = FRAME_LENGTH2;
myrxdata.frmSyncIgn = CSL_MCBSP_FRMSYNC_DETECT;
myrxdata.compand = CSL_MCBSP_COMPAND_OFF_MSB_FIRST;
myrxdata.dataDelay = CSL_MCBSP_DATADELAY_0_BIT;
myrxdata.rjust_dxenable = CSL_MCBSP_RJUSTDXENA_RJUST_RZF;
myrxdata.intEvent = CSL_MCBSP_INTMODE_ON_SYNCERR; // RINTM of SPCR . Value is 2'b11
mytxdata.wordReverse = CSL_MCBSP_32BIT_REVERS_DISABLE;
mytxdata.numPhases = CSL_MCBSP_PHASE_SINGLE;
mytxdata.wordLength1 = CSL_MCBSP_WORDLEN_32;
mytxdata.frmLength1 = FRAME_LENGTH1;
mytxdata.wordLength2 = CSL_MCBSP_WORDLEN_8;
mytxdata.frmLength2 = FRAME_LENGTH2;
mytxdata.frmSyncIgn = CSL_MCBSP_FRMSYNC_DETECT;
mytxdata.compand = CSL_MCBSP_COMPAND_OFF_MSB_FIRST;
mytxdata.dataDelay = CSL_MCBSP_DATADELAY_0_BIT;
mytxdata.rjust_dxenable = CSL_MCBSP_RJUSTDXENA_RJUST_RZF;
mytxdata.intEvent = CSL_MCBSP_INTMODE_ON_FSYNC; //XINTM OF SPCR.Value is 2'b10
myclkset.frmSyncTxMode = CSL_MCBSP_FSCLKMODE_INTERNAL; // Refers to FSXM field of PCR register
myclkset.frmSyncRxMode = CSL_MCBSP_FSCLKMODE_INTERNAL; // Refers to FSRM field of PCR register
// myclkset.frmSyncRxMode = CSL_MCBSP_FSCLKMODE_INTERNAL;
myclkset.clkRxMode = CSL_MCBSP_TXRXCLKMODE_INTERNAL; // Refers to CLKRM field of PCR register
myclkset.clkTxMode = CSL_MCBSP_TXRXCLKMODE_INTERNAL; // Refers to CLKXM field of PCR register
myclkset.frmSyncTxPolarity = CSL_MCBSP_FSPOL_ACTIVE_HIGH; //Refers to FSXP field of PCR register
myclkset.frmSyncRxPolarity = CSL_MCBSP_FSPOL_ACTIVE_HIGH; //Refers to FSRP field of PCR register
myclkset.clkTxPolarity = CSL_MCBSP_CLKPOL_TX_FALLING_EDGE; //Refers to CLKXP field of PCR register
myclkset.clkRxPolarity = CSL_MCBSP_CLKPOL_RX_RISING_EDGE; //Refers to CLKRP field of PCR register
myclkset.srgClkDivide = ClkDiv ; //CLKGDIV OF SRGR
myclkset.srgFrmPulseWidth = FRAME_PULSE_WIDTH; //FWID OF SRGR
myclkset.srgFrmPeriod = FRAME_PERIOD; //FPER OF SRGR
//myclkset.srgInputClkMode = CSL_MCBSP_SRGCLK_CLKS; //CLKSM OF SGRGR i.e External clock source.
myclkset.srgInputClkMode = CSL_MCBSP_SRGCLK_CLKCPU; //Change from external clk to CPU clock
myclkset.srgClkPolarity = CSL_MCBSP_CLKPOL_SRG_RISING_EDGE; //CLKSP OF SRGR
myclkset.srgTxFrmSyncMode = CSL_MCBSP_TXFSMODE_SRG; // FSGM OF SRGR
myclkset.srgClkSync = CSL_MCBSP_CLKGSYNCMODE_OFF; //GSYNC OF SRGR
mymulCh.rxPartition = CSL_MCBSP_PARTMODE_2PARTITION; //All 128 Channels are enabled
mymulCh.txPartition = CSL_MCBSP_PARTMODE_2PARTITION;
mymulCh.rxMulChSel = CSL_MCBSP_MULTI_CHANNEL_RX_EN_ALL; // RMCM =0 in MCR register
mymulCh.txMulChSel = CSL_MCBSP_MULTI_CHANNEL_TX_EN_NO_MASK; //XMCM =2'b01 in MCR reg
mymulCh.rxPartABlk = CSL_MCBSP_PABLK_0;
mymulCh.rxPartBBlk = CSL_MCBSP_PBBLK_1;
mymulCh.txPartABlk = CSL_MCBSP_PABLK_0;
mymulCh.txPartBBlk = CSL_MCBSP_PBBLK_1;
//mySetup.emumode = CSL_MCBSP_EMU_STOP;
mySetup.emumode = CSL_MCBSP_EMU_FREERUN;
mySetup.global = &myglobal;
mySetup.rxdataset = &myrxdata;
mySetup.txdataset = &mytxdata;
mySetup.clkset = &myclkset;
mySetup.mulCh = &mymulCh;
}
Thanks.
Regards,
Steve
Hi Steven,
I found my problem with break point cause EDMA/McBSP stop. That was due to my
Setup.emumode = CSL_MCBSP_EMU_FREERUN; and CSL_MCBSP_EMU_FREERUN = 2. It should be 3. After that change the break point no long cause problem.
Also as Hari mentioned, I would like to make this ping-pong continuous (infinite). And read proper buffer (ping/pong buffers). Could you give us this solution?
Thank you.
Regards,
Steve
Steve/Hari,
Since the McBSP LLD is available in PDK C6657 1_1_1_4 of MCSDK 02_01_01_04, we could switch to that project instead of using the previous McBSP example I attached.
The LLD is well documented and will be updated along with MCSDK package. I am checking with the LLD team to see if/how the EDMA ping/pong operation is supported in the McBSP example. I hope to get the update soon.
At the meanwhile, please take a look at the "MCBSP_LLD_SDS.pdf" file in "C:\ti\pdk_C6657_1_1_1_4\docs" folder and the McBSP digital loopback example in "C:\ti\pdk_C6657_1_1_1_4\packages\ti\drv\exampleProjects" folder as well.
Steven,
I took this code and am presently working on it. This example shows transfer asynchronously. I mean you set tranfer/receive once and wait for completion and send next buffer. If I do IOBUF Read/Write continously in a while loop checking for edmaRxDone-> Set Rx SubmitChan similarly when edmaTxDone comes then set TxSubmitChan. The buffers used in submitChan correspond to a Ping/Pong buffer. And I do this in a while loop infinitely toggling the SubmitChan Buffers. Does this guarantee the data acquistion is continuous. Somewhere in the driver program I am afraid if it shuts down EDMA till the next transfer initiate or disable McBSP. Pl. advise the best way to get Ping/Ping Continuous working on this LLD Project.
In the _drv.c
instHandle->xmtObj.enableHwFifo = FALSE;
instHandle->rcvObj.enableHwFifo = FALSE;
chanHandle->nextLinkParamSetToBeUpdated = 1;
Since we enabled the nextLinkParamSetToBeUpdated, should we give two successive IOBUF read/Writes so that Link gets established? And there is always a delay of two. Pl. advise.
Regards,
Hari
/*
* mcbspMasterDigLpbk.c
*
* This file contains the test / demo code to demonstrate the McBSP driver
* master functionality using Digital Loopback setup. The file configures
* the EVM in master mode.
*
* Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* ========================================================================== */
/* INCLUDE FILES */
/* ========================================================================== */
#include <ti/sysbios/BIOS.h>
#include <xdc/std.h>
#include <ti/sysbios/knl/task.h>
#include <string.h>
#include <ti/sysbios/knl/Queue.h>
#include <xdc/runtime/System.h>
#include <xdc/cfg/global.h>
/* Include EDMA3 Driver */
#include <ti/sdo/edma3/drv/edma3_drv.h>
/* CSL Chip Functional Layer */
#include <ti/csl/csl_chip.h>
/* CSL Cache Functional Layer */
#include <ti/csl/csl_cacheAux.h>
/* CSL CPINTC Include Files. */
#include<ti/csl/csl_cpIntc.h>
/* MCBSP Driver Include File. */
#include <ti/drv/mcbsp/mcbsp_drv.h>
#include <ti/drv/mcbsp/mcbsp_osal.h>
/* PlatformLib Include File */
#include <ti/platform/platform.h>
/* ========================================================================== */
/* EXTERNAL FUNCTIONS */
/* ========================================================================== */
extern EDMA3_DRV_Handle edma3init(unsigned int edma3Id, EDMA3_DRV_Result *);
extern void McbspDevice_init(void);
extern int32_t Osal_dataBufferInitMemory(uint32_t dataBufferSize);
/* FPGA Configuration Misc-1 Register offset */
#define MCBSP_FPGA_MISC_REG_OFFSET (0x0C)
/* ========================================================================== */
/* MACRO DEFINTIONS */
/* ========================================================================== */
#define NUM_BUFS 2 /* Max of 2 outstanding requests */
#define NUM_OF_CHANNELS 24 /* Number of slots to be used */
#define BUFSIZE (80*NUM_OF_CHANNELS) /* 1K of data transceive */
/* Defines the core number responsible for system initialization. */
#define CORE_SYS_INIT 0
/*============================================================================*/
/* GLOBAL VARIABLES */
/*============================================================================*/
/* Shared Memory Variable to ensure synchronizing MCBSP initialization
* with all the other cores. */
/* Created an array to pad the cache line with MCBSP_CACHE_LENGTH size */
#pragma DATA_ALIGN (isMCBSPInitialized, MCBSP_MAX_CACHE_ALIGN)
#pragma DATA_SECTION (isMCBSPInitialized, ".mcbspSharedMem");
volatile Uint32 isMCBSPInitialized[(MCBSP_CACHE_LENGTH / sizeof(Uint32))] = { 0 };
/* Handle to the EDMA driver instance */
#pragma DATA_ALIGN (hEdma, MCBSP_MAX_CACHE_ALIGN)
EDMA3_DRV_Handle hEdma[(MCBSP_CACHE_LENGTH / sizeof(EDMA3_DRV_Handle))] = { NULL };
/* Handle to MCBSP driver instance */
typedef void* Mcbsp_DevHandle;
Mcbsp_DevHandle hMcbspDev;
/* Handle to MCBSP driver channel instance */
typedef void* Mcbsp_ChanHandle;
Mcbsp_ChanHandle hMcbspTxChan;
Mcbsp_ChanHandle hMcbspRxChan;
/* Core Number Identifier */
UInt32 coreNum = 0xFFFF;
/* Array to hold the pointer to the allocated buffers */
void* bufRx[NUM_BUFS];
void* bufTx[NUM_BUFS];
/* Variables to indicate status of EDMA TX and RX requests */
volatile uint32_t edmaTxDone = 0;
volatile uint32_t edmaRxDone = 0;
volatile uint32_t edmaTxCountDone=0;
volatile uint32_t edmaRxCountDone=0;
/**
* \brief Mcbsp Sample rate generator default parameters.
*
*/
Mcbsp_srgConfig mcbspSrgCfg =
{
FALSE, /* No gsync to be used as input is not CLKS */
Mcbsp_ClkSPol_RISING_EDGE, /* Dont care as input clock is not clks */
Mcbsp_SrgClk_CLKCPU, /* McBSP internal clock to be used */
166666667, /* Mcbsp internal clock frequency(PLL-SYSCLK6) */
0 /* frame sync pulse width (val+1) is used */
};
/**
* \brief Mcbsp device creation default parameters.
*
*/
const Mcbsp_Params Mcbsp_PARAMS =
{
Mcbsp_DevMode_McBSP, /* Use the device as MCBSP */
Mcbsp_OpMode_DMAINTERRUPT, /* Use DMA mode of operation */
TRUE, /* cache coherency taken care of by driver */
Mcbsp_EmuMode_SOFT_STOP, /* Soft mode is to be enabled */
Mcbsp_Loopback_DISABLE, /* Loop back mode disabled */
&mcbspSrgCfg, /* sample rate generator configuration */
NULL, /* TX pending buffer queue from application */
NULL, /* TX floating buffer queue in DMA */
NULL, /* RX pending buffer queue from application */
NULL /* RX floating buffer queue in DMA */
};
#pragma DATA_ALIGN(loopJob, MCBSP_MAX_CACHE_ALIGN)
static Int32 loopJob[16] = {
0, 0, 0, 0, 0, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0
};
/**< settings to configure the TX or RX hardware sections */
Mcbsp_DataConfig mcbspChanConfig =
{
Mcbsp_Phase_SINGLE,
Mcbsp_WordLength_32,
Mcbsp_WordLength_32, /* Dont care for single phase*/
NUM_OF_CHANNELS,
NUM_OF_CHANNELS, // Only using single phase, hence num channels is 0
Mcbsp_FrmSync_DETECT,
Mcbsp_DataDelay_1_BIT,
Mcbsp_Compand_OFF_MSB_FIRST,
Mcbsp_BitReversal_DISABLE,
Mcbsp_IntMode_ON_SYNCERR,
Mcbsp_RxJust_RZF, /* Dont care for TX */
Mcbsp_DxEna_OFF
};
/**< clock setup for the TX section */
Mcbsp_ClkSetup mcbspClkConfigTx =
{
Mcbsp_FsClkMode_INTERNAL,
8000, /* 96KHz */
Mcbsp_TxRxClkMode_INTERNAL,
Mcbsp_FsPol_ACTIVE_HIGH,
Mcbsp_ClkPol_RISING_EDGE
};
/**< clock setup for the RX section */
Mcbsp_ClkSetup mcbspClkConfigRx =
{
Mcbsp_FsClkMode_EXTERNAL,
8000, /* 96KHz */
Mcbsp_TxRxClkMode_EXTERNAL,
Mcbsp_FsPol_ACTIVE_HIGH,
Mcbsp_ClkPol_FALLING_EDGE
};
/**< Multi channel setup */
Mcbsp_McrSetup mcbspMultiChanCtrl =
{
Mcbsp_McmMode_ALL_CHAN_ENABLED_UNMASKED,
Mcbsp_PartitionMode_CHAN_0_15,
Mcbsp_PartitionMode_CHAN_16_31,
Mcbsp_PartitionMode_2
};
Mcbsp_ChanParams mcbspChanparamTx =
{
Mcbsp_WordLength_32, /* wordlength configured */
&loopJob[0], /* loop job buffer internal */
8, /* user loopjob length */
NULL, /* global error callback */
NULL, /* edma Handle */
1, /* EDMA event queue */
8, /* hwi number */
Mcbsp_BufferFormat_MULTISLOT_NON_INTERLEAVED,
TRUE, /* FIFO mode enabled */
&mcbspChanConfig, /* channel configuration */
&mcbspClkConfigTx, /* clock configuration */
&mcbspMultiChanCtrl, /* multi channel control */
0x00,
0x00,
0x00,
0x00
};
Mcbsp_ChanParams mcbspChanparamRx =
{
Mcbsp_WordLength_32, /* wordlength configured */
&loopJob[0], /* loop job buffer internal */
8, /* user loopjob length */
NULL, /* global error callback */
NULL, /* edma Handle */
2, /* EDMA event queue */
8, /* hwi number */
Mcbsp_BufferFormat_MULTISLOT_NON_INTERLEAVED,
TRUE, /* FIFO mode enabled */
&mcbspChanConfig, /* channel configuration */
&mcbspClkConfigRx, /* clock configuration */
&mcbspMultiChanCtrl, /* multi channel control */
0x00,
0x00,
0x00,
0x00
};
/* ========================================================================== */
/* FUNCTION DEFINITIONS */
/* ========================================================================== */
/*
* This is the application's callback function. The driver will
* call this function whenever an EDMA I/O operation is over.
*
*/
void mcbspAppCallback(void* arg, Mcbsp_IOBuf *ioBuf)
{
int32_t mode;
int32_t *pmode = (int32_t *)arg;
mode = *pmode;
if (mode == MCBSP_MODE_OUTPUT)
{
edmaTxDone = 1;
edmaTxCountDone++;
}
else if (mode == MCBSP_MODE_INPUT)
{
edmaRxDone = 1;
edmaRxCountDone++;
}
return;
}
void testMcBSPLoop(void);
/*
* \brief This function demostrates the use of Mcbsp using digital loopback
* communication setup.
*
* \param None
*
* \return None
*/
void mcbspDigLpbkApp(UArg arg0, UArg arg1)
{
/**< Mcbsp device params */
Mcbsp_Params mcbspParams;
/**< Mcbsp sample rate configuration parameters */
Mcbsp_srgConfig mcbspSrgParams;
/**< Queue to hold the pending packets received from the application */
Queue_Struct txQueuePendingList, rxQueuePendingList;
/**< Queue to manage floating packets in DMA */
Queue_Struct txQueueFloatingList, rxQueueFloatingList;
uint32_t count = 0, tempCount = 0;
int32_t status = 0, retval = 0;
int32_t txChanMode = MCBSP_MODE_OUTPUT;
int32_t rxChanMode = MCBSP_MODE_INPUT;
uint32_t mcbspTxDone = 0, mcbspRxDone = 0;
Mcbsp_IOBuf txFrame, rxFrame;
/* Initialize the OSAL */
if (Osal_dataBufferInitMemory(BUFSIZE) < 0)
{
System_printf ("Debug(Core %d): Error: Unable to initialize the OSAL. \n", coreNum);
return;
}
/* update EDMA3 handle to channel parameters */
mcbspChanparamTx.edmaHandle = hEdma[0];
mcbspChanparamRx.edmaHandle = hEdma[0];
/* create the pending and floating queue for the TX channel */
Queue_construct(&txQueuePendingList, NULL);
Queue_construct(&txQueueFloatingList, NULL);
/* create the pending and floating queue for the RX channel */
Queue_construct(&rxQueuePendingList, NULL);
Queue_construct(&rxQueueFloatingList, NULL);
/* configure the SRG properties */
/* use Mcbsp intenal clock */
mcbspSrgParams.srgInputClkMode = Mcbsp_SrgClk_CLKCPU;
/* 1 bit width framesync */
mcbspSrgParams.srgFrmPulseWidth = 0;
/* internal clock frequncy */
mcbspSrgParams.srgrInputFreq = 166666667; /* 166.67 MHz - SYSCLK6 */
mcbspParams = Mcbsp_PARAMS;
mcbspParams.mode = Mcbsp_DevMode_McBSP;
mcbspParams.opMode = Mcbsp_OpMode_DMAINTERRUPT;
mcbspParams.enablecache = TRUE;
mcbspParams.emulationMode = Mcbsp_EmuMode_FREE;
mcbspParams.dlbMode = Mcbsp_Loopback_ENABLE;//Mcbsp_Loopback_DISABLE;
mcbspParams.srgSetup = &mcbspSrgParams;
mcbspParams.txQPendingList = &txQueuePendingList;
mcbspParams.txQFloatingList = &txQueueFloatingList;
mcbspParams.rxQPendingList = &rxQueuePendingList;
mcbspParams.rxQFloatingList = &rxQueueFloatingList;
/* Bind the driver instance with device instance */
status = mcbspBindDev(&hMcbspDev, coreNum, &mcbspParams);
if (status != MCBSP_STATUS_COMPLETED)
{
System_printf ("Debug(Core %d): MCBSP LLD Bind Device Failed\n", coreNum);
return;
}
/* Create a RX channel for receiving */
status = mcbspCreateChan(&hMcbspRxChan, hMcbspDev, MCBSP_MODE_INPUT, &mcbspChanparamRx, mcbspAppCallback, &rxChanMode);
if (MCBSP_STATUS_COMPLETED != status)
{
System_printf ("Debug(Core %d): Error: Create Channel (RX) failed\n", coreNum);
return;
}
/* Create a TX channel for the transmission */
status = mcbspCreateChan(&hMcbspTxChan, hMcbspDev, MCBSP_MODE_OUTPUT, &mcbspChanparamTx, mcbspAppCallback, &txChanMode);
if (MCBSP_STATUS_COMPLETED != status)
{
System_printf ("Debug(Core %d): Error: Create Channel (TX) failed\n", coreNum);
return;
}
/* create the buffers required for the TX and RX operations */
for (count = 0; count < (NUM_BUFS); count++)
{
bufTx[count] = (uint8_t *)Osal_mcbspDataBufferMalloc(BUFSIZE);
bufRx[count] = (uint8_t *)Osal_mcbspDataBufferMalloc(BUFSIZE);
if (bufTx[count] == NULL)
{
System_printf ("Debug(Core %d): Error: Tx Buffer (%d) Memory Allocation Failed\n", coreNum, count);
return;
}
if (bufRx[count] == NULL)
{
System_printf ("Debug(Core %d): Error: Rx Buffer (%d) Memory Allocation Failed\n", coreNum, count);
return;
}
}
/* Fill the buffers with known data and transmit the same and
check if the same pattern is received */
for (count = 0; count < (NUM_BUFS); count++)
{
memset((uint8_t *)bufTx[count], 0, BUFSIZE);
for (tempCount = 0; tempCount < BUFSIZE; tempCount++)
{
((uint8_t *)bufTx[count])[tempCount] = (tempCount % 0x100);
}
}
testMcBSPLoop();
}
int edmaSuccessCnt=0;
int edmaDebug=1;
int mcbspRxBufEdmaIndex = 0;
int mcbspRxBufRdIndex = 1;
int mcbspTxBufEdmaIndex = 0;
int mcbspTxBufWrIndex = 1;
void testMcBSPLoop(void)
{
uint32_t count = 0, tempCount = 0, newcount=0;
int32_t status = 0, retval = 0;
int32_t txChanMode = MCBSP_MODE_OUTPUT;
int32_t rxChanMode = MCBSP_MODE_INPUT;
uint32_t mcbspTxDone = 0, mcbspRxDone = 0;
Mcbsp_IOBuf txFrame, rxFrame;
newcount=0;
#if 1
newcount++;
count = newcount & 1;
mcbspRxBufEdmaIndex = (mcbspRxBufEdmaIndex +1)%NUM_BUFS;
mcbspRxBufRdIndex = (mcbspRxBufRdIndex +1)%NUM_BUFS;
mcbspTxBufEdmaIndex = (mcbspTxBufEdmaIndex +1)%NUM_BUFS;
mcbspTxBufWrIndex = (mcbspTxBufWrIndex +1)%NUM_BUFS;
memset((uint8_t *)bufRx[mcbspRxBufEdmaIndex], 0, BUFSIZE);
/* RX frame processing */
rxFrame.cmd = Mcbsp_IOBuf_Cmd_READ;
rxFrame.addr = (void*)bufRx[mcbspRxBufEdmaIndex];
rxFrame.size = BUFSIZE;
rxFrame.arg = (uint32_t) hMcbspRxChan;
rxFrame.status = MCBSP_STATUS_COMPLETED;
rxFrame.misc = 1; /* reserved - used in callback to indicate asynch packet */
status = mcbspSubmitChan(hMcbspRxChan, (void *)&rxFrame);
if (status != MCBSP_STATUS_PENDING)
{
System_printf ("Debug(Core %d): Error: RX buffer submission in iteration-%d FAILED\n", coreNum, newcount);
retval = 1;
}
else
{
//System_printf ("Debug(Core %d): RX buffer in iteration-%d is submitted to MCBSP driver\n", coreNum, newcount);
}
/* TX frame processing */
txFrame.cmd = Mcbsp_IOBuf_Cmd_WRITE;
txFrame.addr = (void*)bufTx[mcbspTxBufEdmaIndex];
txFrame.size = BUFSIZE;
txFrame.arg = (uint32_t)hMcbspTxChan;
txFrame.status = MCBSP_STATUS_COMPLETED;
txFrame.misc = 1; /* reserved - used in callback to indicate asynch packet */
status = mcbspSubmitChan(hMcbspTxChan, (void *)&txFrame);
if (status != MCBSP_STATUS_PENDING)
{
System_printf ("Debug(Core %d): Error: TX frames submission in iteration-%d FAILED\n", coreNum, newcount);
retval = 1;
}
else
{
//System_printf ("Debug(Core %d): TX frames in iteration-%d are submitted to MCBSP driver\n", coreNum, newcount);
}
#endif
/* submit frames to the driver */
while(1)
{
/* Wait for TX and RX processing to complete */
retval = 0;
while (1)
{
Task_sleep(1);
if (edmaTxDone == 1)
{
//System_printf ("Debug(Core %d): EDMA -> Iteration-%d frames are transmitted to TX path\n", coreNum, newcount);
edmaTxDone = 0; /* Reset for next iteration */
mcbspTxDone = 1;
}
if (edmaRxDone == 1)
{
//System_printf ("Debug(Core %d): EDMA -> Iteration-%d frames are received from RX path\n", coreNum, newcount);
edmaRxDone = 0; /* Reset for next iteration */
mcbspRxDone = 1;
}
if ((mcbspTxDone == 1) && (mcbspRxDone == 1))
{
mcbspTxDone = 0; /* Reset for next iteration */
mcbspRxDone = 0; /* Reset for next iteration */
break;
}
}
newcount++;
count = newcount & 1;
mcbspRxBufEdmaIndex = (mcbspRxBufEdmaIndex +1)%NUM_BUFS;
mcbspRxBufRdIndex = (mcbspRxBufRdIndex +1)%NUM_BUFS;
mcbspTxBufEdmaIndex = (mcbspTxBufEdmaIndex +1)%NUM_BUFS;
mcbspTxBufWrIndex = (mcbspTxBufWrIndex +1)%NUM_BUFS;
memset((uint8_t *)bufRx[mcbspRxBufEdmaIndex], 0, BUFSIZE);
/* RX frame processing */
rxFrame.cmd = Mcbsp_IOBuf_Cmd_READ;
rxFrame.addr = (void*)bufRx[mcbspRxBufEdmaIndex];
rxFrame.size = BUFSIZE;
rxFrame.arg = (uint32_t) hMcbspRxChan;
rxFrame.status = MCBSP_STATUS_COMPLETED;
rxFrame.misc = 1; /* reserved - used in callback to indicate asynch packet */
status = mcbspSubmitChan(hMcbspRxChan, (void *)&rxFrame);
if (status != MCBSP_STATUS_PENDING)
{
System_printf ("Debug(Core %d): Error: RX buffer submission in iteration-%d FAILED\n", coreNum, newcount);
retval = 1;
}
else
{
//System_printf ("Debug(Core %d): RX buffer in iteration-%d is submitted to MCBSP driver\n", coreNum, newcount);
}
/* TX frame processing */
txFrame.cmd = Mcbsp_IOBuf_Cmd_WRITE;
txFrame.addr = (void*)bufTx[mcbspTxBufEdmaIndex];
txFrame.size = BUFSIZE;
txFrame.arg = (uint32_t)hMcbspTxChan;
txFrame.status = MCBSP_STATUS_COMPLETED;
txFrame.misc = 1; /* reserved - used in callback to indicate asynch packet */
status = mcbspSubmitChan(hMcbspTxChan, (void *)&txFrame);
if (status != MCBSP_STATUS_PENDING)
{
System_printf ("Debug(Core %d): Error: TX frames submission in iteration-%d FAILED\n", coreNum, newcount);
retval = 1;
}
else
{
//System_printf ("Debug(Core %d): TX frames in iteration-%d are submitted to MCBSP driver\n", coreNum, newcount);
}
/* compare buffer contents */
if(edmaDebug)
{
for (tempCount = 0; tempCount < BUFSIZE; tempCount++)
{
if (((char *)bufTx[mcbspTxBufWrIndex])[tempCount] != ((char *)bufRx[mcbspRxBufRdIndex])[tempCount])
{
System_printf("Debug(Core %d): Error: TX and RX frame data DOES NOT match in iteration-%d\n",
coreNum, count);
System_printf("Debug(Core %d): Error: Buffer index = %d, Tx data = %d, Rx data = %d\n", coreNum,
tempCount, ((char *)bufTx[count])[tempCount], ((char *)bufRx[count])[tempCount]);
retval = 1;
break;
}
}
if (tempCount >= BUFSIZE)
{
edmaSuccessCnt++;
if(edmaDebug) System_printf("Debug(Core %d): TX and RX frames data match in iteration-%d !!![%d, %d, %d, %d]\n", coreNum, newcount,mcbspRxBufEdmaIndex, mcbspRxBufRdIndex, mcbspTxBufEdmaIndex, mcbspTxBufWrIndex);
}
if (retval == 0)
{
//System_printf("Debug(Core %d): MCBSP Digital Loopback Application completed successfully !!!\n", coreNum);
}
else
{
System_printf("Debug(Core %d): MCBSP Digital Loopback application FAILED !!!\n", coreNum);
retval = 0;/* For Debugging */
}
}
}
return;
}
/*
* \brief Void main(Void)
*
* Main function of the sample application. This function calls the
* function to configure the mcbsp instance.
*
* \param None
*
* \return None
*/
Void myStartupFxn(Void)
{
//BIOS_start();
}
Void mcbspmain0(Void);
Void main(void)
{
mcbspmain0();
}
Void mcbspmain0(Void)
{
Task_Params taskParams;
EDMA3_DRV_Result edmaResult = 0;
uint8_t uchValue;
/* Get the core number. */
coreNum = CSL_chipReadReg (CSL_CHIP_DNUM);
#ifdef SIMULATOR_SUPPORT
#warn MCBSP Digital Loopback example is not supported on SIMULATOR !!!
System_printf ("MCBSP Digital Loopback example is not supported on SIMULATOR. Exiting!\n");
return;
#else
System_printf ("Debug(Core %d): Running MCBSP Digital Loopback example on the DEVICE\n", coreNum);
#endif
/* Initialize the system only if the core was configured to do so. */
if (coreNum == CORE_SYS_INIT)
{
System_printf ("Debug(Core %d): System Initialization for MCBSP\n", coreNum);
/* Drive McBSP_AMC_EN# high. Output SLCLKs, TxCLKs, RxCLKs, FSTs, FSRs as Hi-Z.
* These clocks and syncs are tri-stated and McBSP is accessed over 80-pin header */
if (0 != (platform_fpgaWriteConfigReg(MCBSP_FPGA_MISC_REG_OFFSET, 11)))
{
System_printf ("Debug(Core %d): FPGA McBSP_AMC_EN# register WRITE failed \n", coreNum);
return;
}
/* DEBUG: Verify if FPGA register is configured correctly */
if (0 != (platform_fpgaReadConfigReg(MCBSP_FPGA_MISC_REG_OFFSET, &uchValue)))
{
System_printf ("Debug(Core %d): FPGA McBSP_AMC_EN# register READ failed \n", coreNum);
return;
}
if (11 != uchValue)
{
System_printf ("Debug(Core %d): FPGA McBSP_AMC_EN# register setting failed \n", coreNum);
return;
}
else
{
System_printf ("Debug(Core %d): FPGA McBSP_AMC_EN# register is set to %d \n", coreNum, uchValue);
}
/* MCBSP Driver Initialization: This should always be called before
* invoking the MCBSP Driver. */
mcbspInit();
/* Device Specific MCBSP Initializations */
McbspDevice_init();
/* MCBSP Driver is operational at this time. */
System_printf ("Debug(Core %d): MCBSP Driver Initialization Done\n", coreNum);
/* Write to the SHARED memory location at this point in time. The other cores cannot execute
* till the MCBSP Driver is up and running. */
isMCBSPInitialized[0] = 1;
/* The MCBSP IP block has been initialized. We need to writeback the cache here because it will
* ensure that the rest of the cores which are waiting for MCBSP to be initialized would now be
* woken up. */
CACHE_wbL1d ((void *) &isMCBSPInitialized[0], MCBSP_MAX_CACHE_ALIGN, CACHE_FENCE_WAIT);
}
else
{
/* All other cores need to wait for the MCBSP to be initialized before they proceed with the test. */
System_printf ("Debug(Core %d): Waiting for MCBSP to be initialized.\n", coreNum);
/* All other cores loop around forever till the MCBSP is up and running.
* We need to invalidate the cache so that we always read this from the memory. */
while (isMCBSPInitialized[0] == 0)
CACHE_invL1d ((void *) &isMCBSPInitialized[0], MCBSP_MAX_CACHE_ALIGN, CACHE_FENCE_WAIT);
System_printf ("Debug(Core %d): MCBSP can now be used.\n", coreNum);
}
/* Initialize EDMA3 library */
hEdma[0] = edma3init(0, &edmaResult);
if (edmaResult != EDMA3_DRV_SOK)
{
/* Report EDMA Error */
System_printf("Debug(Core %d): EDMA Driver Initialization FAILED\n", coreNum);
}
else
{
System_printf("Debug(Core %d): EDMA Driver Initialization Done\n", coreNum);
}
/* Create the Digital Loopback Application Task */
Task_Params_init(&taskParams);
Task_create(mcbspDigLpbkApp, &taskParams, NULL);
/* Start BIOS */
BIOS_start();
return;
}
/* ========================================================================== */
/* END OF FILE */
/* ========================================================================== */
Hi Steven,
I hacked some code to write EDMA3 PaRAM and get the ping pong buffers to work. But I don't know how to set up EDMA3 transfer completion interrupts. Could give me some help in that area?
Thank you.
Regards,
Steve
Steve,
Glad to hear you are able to make the ping pong buffer working.Did you modify the new McBSL LLD example please?
For the EDMA completion interrupt, I think you might already look at the ping-pong buffering example in EDMA user guide (section 3.4.4).
We can just choose to use the dedicated EDMA channels related to the McBSP RX/TX events. And in each PaRAM set, we can set ITCCHEN/TCCHEN/ITCINTEN to be 0 and set TCINTEN to be 1. The McBSP event will trigger the ping buffer transfer (original PaRAM set). And once the ping buffer transfer completes, the same channel will load the the linked PaRAM set for the pong buffer. And the pong transfer will be triggered by the new McBSP event automatically.
Hope that answers your question.
Hi Steven,
I have a problem with EDMA3 stops without apparent reason. I narrowed it down to my audio packet length. I attached EDMA3 settings here:
AUDIO_FRAME_LEN = 64, EDMS3 settings with ping pong buffer.
AUDIO_FRAME_LEN = 128, EDMS3 settings with ping pong buffer.
The only change is the length. The length only affects EDMA3 settings. What is the problem?
Thank you.
Regards,
Steve
Steve,
May I ask how do you decide "EDMA3 stops without apparent reason" please? Does the EDMA stops in the middle of either ping or pong transfer or does it complete ping transfer but not able to start pong transfer?
Are the EDMA transactions being triggered by McBSP events please? One thing you can check is to remove the McBSP from EDMA and manually trigger the EDMA to see if the transactions happen correctly.
And you said "narrowed it down to my audio packet length". Does it mean the issue only happens when certain length being used in EDMA ParamSet? If so, which length cause the issue and which does not?
Steven,
May I ask how do you decide "EDMA3 stops without apparent reason" please?
Answer: EDMA3 PaRAM is no longer changing.
Does the EDMA stops in the middle of either ping or pong transfer or does it complete ping transfer but not able to start pong transfer?
Answer: EDMA transfered its own buffer, reloaded and transfered ping buffer and reloaded and trasfered pong buffer, then stop.
Are the EDMA transactions being triggered by McBSP events please?
Answer: Yes.
Steve,
Are you able to confirm EDMA transaction stall is due to the McBSP (no new event to EDMA) or the EDMA itself (such as Null PaRAM triggers EMR and SER being set and stalls the further transactions).
And I am a little confused about your Ping Pong buffer PaRAM setup. Are you sure the data transfer happens correctly, even in length=64 case?
For receive, EDMA will read data from the same McBSP register (DRR) and move it to other memory buffer, the srcBIDX and srcCIDX should be 0x0 since the source address (DRR) will remain the same, is it correct? And the same case for transmit (DXR and dstBIDX, dstCIDX).
Could you check with the section 3.4.4 "Ping-Pong buffering" in EDMA user guide to see the PaRAM setup please?
Steven,
In fact, I think RX DMA is working. It continously move data from DDR to memory. If I change DDR value, they go to memory.
My ping pong buffer and everything else working perfactly for 32, 64 sample length, but not 128.
By the way, I am using BFIFO. WNUMEVT and RNUMEVT set to 8.
Thank you.
Regards,
Steve