This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: MLO and U-boot issues

Part Number: PROCESSOR-SDK-AM335X


Hello everyone,

I'm trying to bring up a custom board similar to the BBB with the AM335x and I can see the steady "CCCCC".  Because of a different RAM (Micron MT41K256M16HA-125:E) on my board as on the BBB, I followed these wiki:

_processors.wiki.ti.com/.../Sitara_Linux_Training:_Tuning_the_DDR3_Timings_on_BeagleBoneBlack

in the newest SDK for am335x-evm. When I create an sd-card, I only see this in the terminal:

"U-Boot SPL 2017.01-g590c7d7fe1 (Sep 26 2017 - 18:28:01)" at boot.

/*
 * board.c
 *
 * Board functions for TI AM335X based boards
 *
 * Copyright (C) 2011, Texas Instruments, Incorporated - http://www.ti.com/
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License as
 * published by the Free Software Foundation; either version 2 of
 * the License, or (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR /PURPOSE.  See the
 * GNU General Public License for more details.
 */

#include <common.h>
#include <errno.h>
#include <spl.h>
#include <asm/arch/cpu.h>
#include <asm/arch/hardware.h>
#include <asm/arch/omap.h>
#include <asm/arch/ddr_defs.h>
#include <asm/arch/clock.h>
#include <asm/arch/gpio.h>
#include <asm/arch/mmc_host_def.h>
#include <asm/arch/sys_proto.h>
#include <asm/io.h>
#include <asm/emif.h>
#include <asm/gpio.h>
#include <i2c.h>
#include <miiphy.h>
#include <cpsw.h>
#include "board.h"
#include "pmic.h"
#include "tps65217.h"

DECLARE_GLOBAL_DATA_PTR;

static struct wd_timer *wdtimer = (struct wd_timer *)WDT_BASE;
#if defined(CONFIG_SPL_BUILD)
static struct uart_sys *uart_base = (struct uart_sys *)DEFAULT_UART_BASE;
#endif

/* MII mode defines */
#define MII_MODE_ENABLE		0x0


static struct ctrl_dev *cdev = (struct ctrl_dev *)CTRL_DEVICE_BASE;

static struct am335x_baseboard_id __attribute__((section (".data"))) header;

/* UART Defines */
#if defined(CONFIG_SPL_BUILD)
/**
 * tps65217_reg_read() - Generic function that can read a TPS65217 register
 * @src_reg:          Source register address
 * @src_val:          Address of destination variable
 */

unsigned char tps65217_reg_read(uchar src_reg, uchar *src_val)
{
        if (i2c_read(TPS65217_CHIP_PM, src_reg, 1, src_val, 1))
                return 1;
        return 0;
}

/**
 *  tps65217_reg_write() - Generic function that can write a TPS65217 PMIC
 *                         register or bit field regardless of protection
 *                         level.
 *
 *  @prot_level:        Register password protection.
 *                      use PROT_LEVEL_NONE, PROT_LEVEL_1, or PROT_LEVEL_2
 *  @dest_reg:          Register address to write.
 *  @dest_val:          Value to write.
 *  @mask:              Bit mask (8 bits) to be applied.  Function will only
 *                      change bits that are set in the bit mask.
 *
 *  @return:            0 for success, 1 for failure.
 */
int tps65217_reg_write(uchar prot_level, uchar dest_reg,
        uchar dest_val, uchar mask)
{
        uchar read_val;
        uchar xor_reg;

        /* if we are affecting only a bit field, read dest_reg and apply the mask */
        if (mask != MASK_ALL_BITS) {
                if (i2c_read(TPS65217_CHIP_PM, dest_reg, 1, &read_val, 1))
                        return 1;
                read_val &= (~mask);
                read_val |= (dest_val & mask);
                dest_val = read_val;
        }

        if (prot_level > 0) {
                xor_reg = dest_reg ^ PASSWORD_UNLOCK;
                if (i2c_write(TPS65217_CHIP_PM, PASSWORD, 1, &xor_reg, 1))
                        return 1;
        }

        if (i2c_write(TPS65217_CHIP_PM, dest_reg, 1, &dest_val, 1))
                return 1;

        if (prot_level == PROT_LEVEL_2) {
                if (i2c_write(TPS65217_CHIP_PM, PASSWORD, 1, &xor_reg, 1))
                        return 1;

                if (i2c_write(TPS65217_CHIP_PM, dest_reg, 1, &dest_val, 1))
                        return 1;
        }

        return 0;
}

int tps65217_voltage_update(unsigned char dc_cntrl_reg, unsigned char volt_sel)
{
        if ((dc_cntrl_reg != DEFDCDC1) && (dc_cntrl_reg != DEFDCDC2)
                && (dc_cntrl_reg != DEFDCDC3))
                return 1;

        /* set voltage level */
        if (tps65217_reg_write(PROT_LEVEL_2, dc_cntrl_reg, volt_sel, MASK_ALL_BITS))
                return 1;

        /* set GO bit to initiate voltage transition */
        if (tps65217_reg_write(PROT_LEVEL_2, DEFSLEW, DCDC_GO, DCDC_GO))
                return 1;

        return 0;
}


#define UART_RESET		(0x1 << 1)
#define UART_CLK_RUNNING_MASK	0x1
#define UART_SMART_IDLE_EN	(0x1 << 0x3)

static void rtc32k_enable(void)
{
	struct rtc_regs *rtc = (struct rtc_regs *)AM335X_RTC_BASE;

	/*
	 * Unlock the RTC's registers.  For more details please see the
	 * RTC_SS section of the TRM.  In order to unlock we need to
	 * write these specific values (keys) in this order.
	 */
	writel(0x83e70b13, &rtc->kick0r);
	writel(0x95a4f1e0, &rtc->kick1r);

	/* Enable the RTC 32K OSC by setting bits 3 and 6. */
	writel((1 << 3) | (1 << 6), &rtc->osc);
}

static const struct ddr_data ddr2_data = {
	.datardsratio0 = ((MT47H128M16RT25E_RD_DQS<<30) |
			  (MT47H128M16RT25E_RD_DQS<<20) |
			  (MT47H128M16RT25E_RD_DQS<<10) |
			  (MT47H128M16RT25E_RD_DQS<<0)),
	.datawdsratio0 = ((MT47H128M16RT25E_WR_DQS<<30) |
			  (MT47H128M16RT25E_WR_DQS<<20) |
			  (MT47H128M16RT25E_WR_DQS<<10) |
			  (MT47H128M16RT25E_WR_DQS<<0)),
	.datawiratio0 = ((MT47H128M16RT25E_PHY_WRLVL<<30) |
			 (MT47H128M16RT25E_PHY_WRLVL<<20) |
			 (MT47H128M16RT25E_PHY_WRLVL<<10) |
			 (MT47H128M16RT25E_PHY_WRLVL<<0)),
	.datagiratio0 = ((MT47H128M16RT25E_PHY_GATELVL<<30) |
			 (MT47H128M16RT25E_PHY_GATELVL<<20) |
			 (MT47H128M16RT25E_PHY_GATELVL<<10) |
			 (MT47H128M16RT25E_PHY_GATELVL<<0)),
	.datafwsratio0 = ((MT47H128M16RT25E_PHY_FIFO_WE<<30) |
			  (MT47H128M16RT25E_PHY_FIFO_WE<<20) |
			  (MT47H128M16RT25E_PHY_FIFO_WE<<10) |
			  (MT47H128M16RT25E_PHY_FIFO_WE<<0)),
	.datawrsratio0 = ((MT47H128M16RT25E_PHY_WR_DATA<<30) |
			  (MT47H128M16RT25E_PHY_WR_DATA<<20) |
			  (MT47H128M16RT25E_PHY_WR_DATA<<10) |
			  (MT47H128M16RT25E_PHY_WR_DATA<<0)),
	.datauserank0delay = MT47H128M16RT25E_PHY_RANK0_DELAY,
	.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct cmd_control ddr2_cmd_ctrl_data = {
	.cmd0csratio = MT47H128M16RT25E_RATIO,
	.cmd0dldiff = MT47H128M16RT25E_DLL_LOCK_DIFF,
	.cmd0iclkout = MT47H128M16RT25E_INVERT_CLKOUT,

	.cmd1csratio = MT47H128M16RT25E_RATIO,
	.cmd1dldiff = MT47H128M16RT25E_DLL_LOCK_DIFF,
	.cmd1iclkout = MT47H128M16RT25E_INVERT_CLKOUT,

	.cmd2csratio = MT47H128M16RT25E_RATIO,
	.cmd2dldiff = MT47H128M16RT25E_DLL_LOCK_DIFF,
	.cmd2iclkout = MT47H128M16RT25E_INVERT_CLKOUT,
};

static const struct emif_regs ddr2_emif_reg_data = {
	.sdram_config = MT47H128M16RT25E_EMIF_SDCFG,
	.ref_ctrl = MT47H128M16RT25E_EMIF_SDREF,
	.sdram_tim1 = MT47H128M16RT25E_EMIF_TIM1,
	.sdram_tim2 = MT47H128M16RT25E_EMIF_TIM2,
	.sdram_tim3 = MT47H128M16RT25E_EMIF_TIM3,
	.emif_ddr_phy_ctlr_1 = MT47H128M16RT25E_EMIF_READ_LATENCY,
};

static const struct ddr_data ddr3_data = {
	.datardsratio0 = MT41J128MJT125_RD_DQS,
	.datawdsratio0 = MT41J128MJT125_WR_DQS,
	.datafwsratio0 = MT41J128MJT125_PHY_FIFO_WE,
	.datawrsratio0 = MT41J128MJT125_PHY_WR_DATA,
	.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct ddr_data ddr3_beagleblack_data = {
	.datardsratio0 = MT41K256M16HA125E_RD_DQS,
 	.datawdsratio0 = MT41K256M16HA125E_WR_DQS,
	.datafwsratio0 = MT41K256M16HA125E_PHY_FIFO_WE,
	.datawrsratio0 = MT41K256M16HA125E_PHY_WR_DATA,
	.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct ddr_data ddr3_evm_data = {
	.datardsratio0 = MT41J512M8RH125_RD_DQS,
	.datawdsratio0 = MT41J512M8RH125_WR_DQS,
	.datafwsratio0 = MT41J512M8RH125_PHY_FIFO_WE,
	.datawrsratio0 = MT41J512M8RH125_PHY_WR_DATA,
	.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct cmd_control ddr3_cmd_ctrl_data = {
	.cmd0csratio = MT41J128MJT125_RATIO,
	.cmd0dldiff = MT41J128MJT125_DLL_LOCK_DIFF,
	.cmd0iclkout = MT41J128MJT125_INVERT_CLKOUT,

	.cmd1csratio = MT41J128MJT125_RATIO,
	.cmd1dldiff = MT41J128MJT125_DLL_LOCK_DIFF,
	.cmd1iclkout = MT41J128MJT125_INVERT_CLKOUT,

	.cmd2csratio = MT41J128MJT125_RATIO,
	.cmd2dldiff = MT41J128MJT125_DLL_LOCK_DIFF,
	.cmd2iclkout = MT41J128MJT125_INVERT_CLKOUT,
};

static const struct cmd_control ddr3_beagleblack_cmd_ctrl_data = {
	.cmd0csratio = MT41K256M16HA125E_RATIO,
	.cmd0dldiff = MT41K256M16HA125E_DLL_LOCK_DIFF,
	.cmd0iclkout = MT41K256M16HA125E_INVERT_CLKOUT,

	.cmd1csratio = MT41K256M16HA125E_RATIO,
	.cmd1dldiff = MT41K256M16HA125E_DLL_LOCK_DIFF,
	.cmd1iclkout = MT41K256M16HA125E_INVERT_CLKOUT,

	.cmd2csratio = MT41K256M16HA125E_RATIO,
	.cmd2dldiff = MT41K256M16HA125E_DLL_LOCK_DIFF,
	.cmd2iclkout = MT41K256M16HA125E_INVERT_CLKOUT,
};

static const struct cmd_control ddr3_evm_cmd_ctrl_data = {
	.cmd0csratio = MT41J512M8RH125_RATIO,
	.cmd0dldiff = MT41J512M8RH125_DLL_LOCK_DIFF,
	.cmd0iclkout = MT41J512M8RH125_INVERT_CLKOUT,

	.cmd1csratio = MT41J512M8RH125_RATIO,
	.cmd1dldiff = MT41J512M8RH125_DLL_LOCK_DIFF,
	.cmd1iclkout = MT41J512M8RH125_INVERT_CLKOUT,

	.cmd2csratio = MT41J512M8RH125_RATIO,
	.cmd2dldiff = MT41J512M8RH125_DLL_LOCK_DIFF,
	.cmd2iclkout = MT41J512M8RH125_INVERT_CLKOUT,
};

static struct emif_regs ddr3_emif_reg_data = {
	.sdram_config = MT41J128MJT125_EMIF_SDCFG,
	.ref_ctrl = MT41J128MJT125_EMIF_SDREF,
	.sdram_tim1 = MT41J128MJT125_EMIF_TIM1,
	.sdram_tim2 = MT41J128MJT125_EMIF_TIM2,
	.sdram_tim3 = MT41J128MJT125_EMIF_TIM3,
	.zq_config = MT41J128MJT125_ZQ_CFG,
	.emif_ddr_phy_ctlr_1 = MT41J128MJT125_EMIF_READ_LATENCY |
				PHY_EN_DYN_PWRDN,
};

static struct emif_regs ddr3_beagleblack_emif_reg_data = {
	.sdram_config = MT41K256M16HA125E_EMIF_SDCFG,
	.ref_ctrl = MT41K256M16HA125E_EMIF_SDREF,
	.sdram_tim1 = MT41K256M16HA125E_EMIF_TIM1,
	.sdram_tim2 = MT41K256M16HA125E_EMIF_TIM2,
	.sdram_tim3 = MT41K256M16HA125E_EMIF_TIM3,
	.zq_config = MT41K256M16HA125E_ZQ_CFG,
	.emif_ddr_phy_ctlr_1 = MT41K256M16HA125E_EMIF_READ_LATENCY,
};

static struct emif_regs ddr3_evm_emif_reg_data = {
	.sdram_config = MT41J512M8RH125_EMIF_SDCFG,
	.ref_ctrl = MT41J512M8RH125_EMIF_SDREF,
	.sdram_tim1 = MT41J512M8RH125_EMIF_TIM1,
	.sdram_tim2 = MT41J512M8RH125_EMIF_TIM2,
	.sdram_tim3 = MT41J512M8RH125_EMIF_TIM3,
	.zq_config = MT41J512M8RH125_ZQ_CFG,
	.emif_ddr_phy_ctlr_1 = MT41J512M8RH125_EMIF_READ_LATENCY |
				PHY_EN_DYN_PWRDN,
};

static const struct ddr_data ddr3_bbb_data = {
.datardsratio0 = MT41K256M16HA125ET_RD_DQS,
.datawdsratio0 = MT41K256M16HA125ET_WR_DQS,
.datafwsratio0 = MT41K256M16HA125ET_PHY_FIFO_WE,
.datawrsratio0 = MT41K256M16HA125ET_PHY_WR_DATA,
.datadldiff0 = PHY_DLL_LOCK_DIFF,
};

static const struct cmd_control ddr3_bbb_cmd_ctrl_data = {
.cmd0csratio = MT41K256M16HA125ET_RATIO,
.cmd0dldiff = MT41K256M16HA125ET_DLL_LOCK_DIFF,
.cmd0iclkout = MT41K256M16HA125ET_INVERT_CLKOUT,
.cmd1csratio = MT41K256M16HA125ET_RATIO,
.cmd1dldiff = MT41K256M16HA125ET_DLL_LOCK_DIFF,
.cmd1iclkout = MT41K256M16HA125ET_INVERT_CLKOUT,
.cmd2csratio = MT41K256M16HA125ET_RATIO,
.cmd2dldiff = MT41K256M16HA125ET_DLL_LOCK_DIFF,
.cmd2iclkout = MT41K256M16HA125ET_INVERT_CLKOUT,
};

static struct emif_regs ddr3_bbb_emif_reg_data = {
.sdram_config = MT41K256M16HA125ET_EMIF_SDCFG,
.ref_ctrl = MT41K256M16HA125ET_EMIF_SDREF,
.sdram_tim1 = MT41K256M16HA125ET_EMIF_TIM1,
.sdram_tim2 = MT41K256M16HA125ET_EMIF_TIM2,
.sdram_tim3 = MT41K256M16HA125ET_EMIF_TIM3,
.zq_config = MT41K256M16HA125ET_ZQ_CFG,
.emif_ddr_phy_ctlr_1 = MT41K256M16HA125ET_EMIF_READ_LATENCY | PHY_EN_DYN_PWRDN,
};


void am33xx_spl_board_init(void)
{
	int mpu_vdd, mpu_pll, sil_rev;
	uchar pmic_status_reg;
	int usb_cur_lim;

	/* Assume PG 1.0 */
	mpu_pll = MPUPLL_M_720;

	sil_rev = readl(&cdev->deviceid) >> 28;
	if (sil_rev == 1)
		/* PG 2.0, efuse may not be set. */
		mpu_pll = MPUPLL_M_800;
	else if (sil_rev >= 2) {
		/* Check what the efuse says our max speed is. */
		int efuse_arm_mpu_max_freq;
		efuse_arm_mpu_max_freq = readl(&cdev->efuse_sma);
		if ((efuse_arm_mpu_max_freq & DEVICE_ID_MASK) ==
				AM335X_ZCZ_1000)
			mpu_pll = MPUPLL_M_1000;
		else if ((efuse_arm_mpu_max_freq & DEVICE_ID_MASK) ==
				AM335X_ZCZ_800)
			mpu_pll = MPUPLL_M_800;
	}

	if (i2c_probe(TPS65217_CHIP_PM))
		return;

	if (tps65217_reg_read(STATUS, &pmic_status_reg))
		return;

	/*
	 * Increase USB current limit to 1300mA or 1800mA and set
	 * the MPU voltage controller as needed.
	 */
	if (mpu_pll == MPUPLL_M_1000) {
		usb_cur_lim = USB_INPUT_CUR_LIMIT_1800MA;
		mpu_vdd = DCDC_VOLT_SEL_1325MV;
	} else {
		usb_cur_lim = USB_INPUT_CUR_LIMIT_1300MA;
		mpu_vdd = DCDC_VOLT_SEL_1275MV;
	}

	if (tps65217_reg_write(PROT_LEVEL_NONE, POWER_PATH,
			       usb_cur_lim, USB_INPUT_CUR_LIMIT_MASK))
		printf("tps65217_reg_write failure\n");


	/* Set DCDC3 (CORE) voltage to 1.125V */
	if (tps65217_voltage_update(DEFDCDC3, DCDC_VOLT_SEL_1125MV)) {
		printf("tps65217_voltage_update failure\n");
		return;
	}

	/* Set CORE Frequency to what we detected */
	core_pll_config(OPP_100);

	/* Set DCDC2 (MPU) voltage to 1.275V */
	if (tps65217_voltage_update(DEFDCDC2, mpu_vdd)) {
		printf("tps65217_voltage_update failure\n");
		return;
	}

	/* Set MPU Frequency to what we detected */
	mpu_pll_config(mpu_pll);

	/* 
	 * Set LDO3, LDO4 output voltage to 3.3V for Beaglebone.
	 */
	if (tps65217_reg_write(PROT_LEVEL_2, DEFLS1,
		       LDO_VOLTAGE_OUT_3_3, LDO_MASK))
		printf("tps65217_reg_write failure\n");

	if (tps65217_reg_write(PROT_LEVEL_2, DEFLS2,
		       LDO_VOLTAGE_OUT_3_3, LDO_MASK))
		printf("tps65217_reg_write failure\n");

	if (!(pmic_status_reg & PWR_SRC_AC_BITMASK)) {
		printf("No AC power, disabling frequency switch\n");
		return;
	}
}
#endif

/*
 * early system init of muxing and clocks.
 */
void s_init(void)
{
	volatile int myVar = 1;
	__maybe_unused struct am335x_baseboard_id header;

	/* WDT1 is already running when the bootloader gets control
	 * Disable it to avoid "random" resets
	 */
	writel(0xAAAA, &wdtimer->wdtwspr);
	while (readl(&wdtimer->wdtwwps) != 0x0)
		;
	writel(0x5555, &wdtimer->wdtwspr);
	while (readl(&wdtimer->wdtwwps) != 0x0)
		;

#if defined(CONFIG_SPL_BUILD)
	/* Setup the PLLs and the clocks for the peripherals */
	pll_init();

	/* Enable RTC32K clock */
	rtc32k_enable();

	/* UART softreset */
	u32 regVal;

#ifdef CONFIG_SERIAL1
	enable_uart0_pin_mux();
#endif /* CONFIG_SERIAL1 */
#ifdef CONFIG_SERIAL2
	enable_uart1_pin_mux();
#endif /* CONFIG_SERIAL2 */
#ifdef CONFIG_SERIAL3
	enable_uart2_pin_mux();
#endif /* CONFIG_SERIAL3 */
#ifdef CONFIG_SERIAL4
	enable_uart3_pin_mux();
#endif /* CONFIG_SERIAL4 */
#ifdef CONFIG_SERIAL5
	enable_uart4_pin_mux();
#endif /* CONFIG_SERIAL5 */
#ifdef CONFIG_SERIAL6
	enable_uart5_pin_mux();
#endif /* CONFIG_SERIAL6 */

	regVal = readl(&uart_base->uartsyscfg);
	regVal |= UART_RESET;
	writel(regVal, &uart_base->uartsyscfg);
	while ((readl(&uart_base->uartsyssts) &
		UART_CLK_RUNNING_MASK) != UART_CLK_RUNNING_MASK)
		;

	/* Disable smart idle */
	regVal = readl(&uart_base->uartsyscfg);
	regVal |= UART_SMART_IDLE_EN;
	writel(regVal, &uart_base->uartsyscfg);

	gd = &gdata;
	preloader_console_init();

	enable_i2c0_pin_mux();
	i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);

	config_ddr(400, MT41K256M16HA125ET_IOCTRL_VALUE, &ddr3_bbb_data,
		   &ddr3_bbb_cmd_ctrl_data, &ddr3_bbb_emif_reg_data);
	while(myVar);
#endif
}

/*
 * Basic board specific setup.  Pinmux has been handled already.
 */
int board_init(void)
{
	i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);

	gd->bd->bi_boot_params = PHYS_DRAM_1 + 0x100;

	gpmc_init();

	return 0;
}

#ifdef CONFIG_BOARD_LATE_INIT
int board_late_init(void)
{
#ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG

	/* Now set variables based on board. */
	setenv("board_name", "A335BONE\0");
#endif

	return 0;
}
#endif

#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
	(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
static void cpsw_control(int enabled)
{
	/* VTP can be added here */

	return;
}

static struct cpsw_slave_data cpsw_slaves[] = {
	{
		.slave_reg_ofs	= 0x208,
		.sliver_reg_ofs	= 0xd80,
		.phy_id		= 0,
	},
	{
		.slave_reg_ofs	= 0x308,
		.sliver_reg_ofs	= 0xdc0,
		.phy_id		= 1,
	},
};

static struct cpsw_platform_data cpsw_data = {
	.mdio_base		= AM335X_CPSW_MDIO_BASE,
	.cpsw_base		= AM335X_CPSW_BASE,
	.mdio_div		= 0xff,
	.channels		= 8,
	.cpdma_reg_ofs		= 0x800,
	.slaves			= 1,
	.slave_data		= cpsw_slaves,
	.ale_reg_ofs		= 0xd00,
	.ale_entries		= 1024,
	.host_port_reg_ofs	= 0x108,
	.hw_stats_reg_ofs	= 0x900,
	.mac_control		= (1 << 5),
	.control		= cpsw_control,
	.host_port_num		= 0,
	.version		= CPSW_CTRL_VERSION_2,
};
#endif

#if defined(CONFIG_DRIVER_TI_CPSW) || \
	(defined(CONFIG_USB_ETHER) && defined(CONFIG_MUSB_GADGET))
int board_eth_init(bd_t *bis)
{
	int rv, n = 0;
	uint8_t mac_addr[6];
	uint32_t mac_hi, mac_lo;

	/* try reading mac address from efuse */
	mac_lo = readl(&cdev->macid0l);
	mac_hi = readl(&cdev->macid0h);
	mac_addr[0] = mac_hi & 0xFF;
	mac_addr[1] = (mac_hi & 0xFF00) >> 8;
	mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
	mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
	mac_addr[4] = mac_lo & 0xFF;
	mac_addr[5] = (mac_lo & 0xFF00) >> 8;

#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
	(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
	if (!getenv("ethaddr")) {
		printf("<ethaddr> not set. Validating first E-fuse MAC\n");

		if (is_valid_ether_addr(mac_addr))
			eth_setenv_enetaddr("ethaddr", mac_addr);
	}

	writel(MII_MODE_ENABLE, &cdev->miisel);
	cpsw_slaves[0].phy_if = cpsw_slaves[1].phy_if =
			PHY_INTERFACE_MODE_MII;

	rv = cpsw_register(&cpsw_data);
	if (rv < 0)
		printf("Error %d registering CPSW switch\n", rv);
	else
		n += rv;
#endif
#if defined(CONFIG_USB_ETHER) && \
	(!defined(CONFIG_SPL_BUILD) || defined(CONFIG_SPL_USBETH_SUPPORT))
	if (is_valid_ether_addr(mac_addr))
		eth_setenv_enetaddr("usbnet_devaddr", mac_addr);

	rv = usb_eth_initialize(bis);
	if (rv < 0)
		printf("Error %d registering USB_ETHER\n", rv);
	else
		n += rv;
#endif
	return n;
}
#endif

After building my own u-boot (command:"make u-boot") and replacing the MLO and u-boot.img, nothing appears at boot on the terminal.

I also tried to enable debug (#define DEBUG in am335x_evm.h), but nothing is vissible.

I read in another thread, that the wiki is a kind of obsolet for the current SDK. If that is correct, is somewhere a current version? Do I only have to replace the MLO and the u-boot.img? Where I have to define the DEBUG?

Thanks very much for your help.

Kind regards

Eric

  • Do you have an ID EEPROM on your board? If not, you will have to skip or hardcode the EEPROM check in the MLO source code.
  • Hi Biser,

    thank you for your fast answer. I have an eeprom, but I would nevertheless try to disable it. Could you tell me which files I have to edit?

    By the way, should there not be an error or some output? Where can I enable it? I add the '#define DEBUG to the am335x board.c file, but there is only the output of the current u-boot?!

    Thanks very much for your help.

    Kind regards

    Eric

  • Hello Eric,

    When you #define DEBUG in am335x_evm.h didn't you got the u-boot-spl section `.data' will not fit in region `.sram' error?

    Best regards,
    Kemal

  • Hello Kemal,

    I only get this output, then nothing more:

    U-Boot SPL 2017.01-00360-gc6c77f9-dirty (Oct 11 2017 - 17:41:14)

    Any other ideas, what could be the problem? It the word "dirty" in the u-boot right?

    Thanks very much.

    Kind regards

    Eric

    3771.am335x_evm.h

  • "dirty" means that you have uncommitted changes in git. Can you put the #define DEBUG under #define CONFIG_AM33XX and retry?
  • Hi Kemal,

    I put it after #define CONFIG_AM33XX but the result is just the same.

    Here are my steps, maybe I just missed something?!

    - Create U-boot

    - Create sd-card

    copy MLO and u-boot.img to boot-partition

    eric@eric-VirtualBox:~/ti-processor-sdk-linux-am335x-evm-04.01.00.06/bin$ sudo ./create-sdcard.sh 
    
    
    ################################################################################
    
    This script will create a bootable SD card from custom or pre-built binaries.
    
    The script must be run with root permissions and from the bin directory of
    the SDK
    
    Example:
     $ sudo ./create-sdcard.sh
    
    Formatting can be skipped if the SD card is already formatted and
    partitioned properly.
    
    ################################################################################
    
    
    Available Drives to write images to: 
    
    #  major   minor    size   name 
    1:   8       16    7655424 sdb
     
    Enter Device Number or n to exit: 1
     
    sdb was selected
    
    /dev/sdb is an sdx device
    Unmounting the sdb drives
     unmounted /dev/sdb1
     unmounted /dev/sdb2
    Current size of sdb1 71680 bytes
    Current size of sdb2 7566336 bytes
    
    ################################################################################
    
    	Select 2 partitions if only need boot and rootfs (most users).
    	Select 3 partitions if need SDK & other content on SD card.  This is
            usually used by device manufacturers with access to partition tarballs.
    
    	****WARNING**** continuing will erase all data on sdb
    
    ################################################################################
    
    Number of partitions needed [2/3] : 2
    
     
    Now partitioning sdb with 2 partitions...
     
    
    ################################################################################
    
    		Now making 2 partitions
    
    ################################################################################
    
    1024+0 records in
    1024+0 records out
    1048576 bytes (1.0 MB) copied, 2.53352 s, 414 kB/s
    Disk /dev/sdb doesn't contain a valid partition table
    DISK SIZE - 7839154176 bytes
    
    ################################################################################
    
    		Partitioning Boot
    
    ################################################################################
    mkfs.fat 3.0.26 (2014-03-07)
    mkfs.fat: warning - lowercase labels might not work properly with DOS or Windows
    
    ################################################################################
    
    		Partitioning rootfs
    
    ################################################################################
    mke2fs 1.42.9 (4-Feb-2014)
    Filesystem label=rootfs
    OS type: Linux
    Block size=4096 (log=2)
    Fragment size=4096 (log=2)
    Stride=0 blocks, Stripe width=0 blocks
    473280 inodes, 1891584 blocks
    94579 blocks (5.00%) reserved for the super user
    First data block=0
    Maximum filesystem blocks=1937768448
    58 block groups
    32768 blocks per group, 32768 fragments per group
    8160 inodes per group
    Superblock backups stored on blocks: 
    	32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632
    
    Allocating group tables: done                            
    Writing inode tables: done                            
    Creating journal (32768 blocks): done
    Writing superblocks and filesystem accounting information: done 
    
    
    
    ################################################################################
    
       Partitioning is now done
       Continue to install filesystem or select 'n' to safe exit
    
       **Warning** Continuing will erase files any files in the partitions
    
    ################################################################################
    
    
    Would you like to continue? [y/n] : y
    
     
    mkdir: cannot create directory '/home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/bin/tmp': File exists
     
    Mount the partitions 
    mkdir: cannot create directory 'boot': File exists
    mkdir: cannot create directory 'rootfs': File exists
     
    Emptying partitions 
     
    
    Syncing....
    
    ################################################################################
    
    	Choose file path to install from
    
    	1 ) Install pre-built images from SDK
    	2 ) Enter in custom boot and rootfs file paths
    
    ################################################################################
    
    Choose now [1/2] : 2
    
     
    
    ################################################################################
    
      For U-boot and MLO
    
      If files are located in Tarball write complete path including the file name.
          e.x. $:  /home/user/MyCustomTars/boot.tar.xz
    
      If files are located in a directory write the directory path
          e.x. $: /ti-sdk/board-support/prebuilt-images/
    
      NOTE: Not all platforms will have an MLO file and this file can
            be ignored for platforms that do not support an MLO.
    
      Update: The proper location for the kernel image and device tree
              files have moved from the boot partition to the root filesystem.
    
    ################################################################################
    
    Enter path for Boot Partition : /home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/board-support/u-boot-2017.01+gitAUTOINC+590c7d7fe1-g590c7d7fe1/
    
    Directory exists
    
    This directory contains:
    Kbuild	      TISDK-README  doc       scripts		u-boot.bin
    Kconfig       api	    drivers   snapshot.commit	u-boot.cfg
    Licenses      arch	    dts       spl		u-boot.cfg.configs
    MAINTAINERS   board	    examples  test		u-boot.dtb
    MLO	      cmd	    fs	      tools		u-boot.img
    MLO.byteswap  common	    include   u-boot		u-boot.lds
    Makefile      config.mk     lib       u-boot-dtb.bin	u-boot.map
    README	      configs	    net       u-boot-dtb.img	u-boot.srec
    System.map    disk	    post      u-boot-nodtb.bin	u-boot.sym
    
    Is this correct? [y/n] : y
    
    
    ################################################################################
    
       For Kernel Image and Device Trees files
    
        What would you like to do?
         1) Reuse kernel image and device tree files found in the selected rootfs.
         2) Provide a directory that contains the kernel image and device tree files
            to be used.
    
    ################################################################################
    
    Choose option 1 or 2 : 1
    
     
    Reusing kernel and dt files from the rootfs's boot directory
     
    
    
    ################################################################################
    
       For Rootfs partition
    
       If files are located in Tarball write complete path including the file name.
          e.x. $:  /home/user/MyCustomTars/rootfs.tar.xz
    
      If files are located in a directory write the directory path
          e.x. $: /ti-sdk/targetNFS/
    
    ################################################################################
    
    Enter path for Rootfs Partition : /home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/targetNFS/
    
    This directory contains:
    bin   dev  home     lib    mnt	proc  sbin  sys  usr  www
    boot  etc  include  media  opt	run   srv   tmp  var
    
    Is this correct? [y/n] : y
    
    ################################################################################
    
    	Copying files now... will take minutes
    
    ################################################################################
    
    Copying boot partition
    
    cp: target 'boot/MLO' is not a directory
    MLO copied
    
    
    cp: target 'boot/u-boot.img' is not a directory
    u-boot.img copied
    
    
    Copying rootfs System partition
    1559324 /  1554196 copied 
    
    Syncing...
     
    Un-mount the partitions 
     
    Remove created temp directories 
     
    Operation Finished
     
    eric@eric-VirtualBox:~/ti-processor-sdk-linux-am335x-evm-04.01.00.06/bin$ 
    
    

    Do you have any other ideas?

    Thanks very much for your help.

    Edit: Could it be, that this while-loop is a problem:


        config_ddr(400, MT41K256M16HA125ET_IOCTRL_VALUE, &ddr3_bbb_data,
               &ddr3_bbb_cmd_ctrl_data, &ddr3_bbb_emif_reg_data);
        while(myVar);
    #endif
    }

    I add this because of the information on this site: _http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Tuning_the_DDR3_Timings_on_BeagleBoneBlack

    maybe it is obsolet?!

    Kind regards

    Eric

  • Hello Kemal,

    I've found the mistake. I copied from git two directories (sitara-board-port-linux and sitara-board-port-uboot) and changed values inside of them but it didnt make any difference.
    When I add the #define debug to am335x_evm.h now, I get the this error:
    oard-support/u-boot-2017.01+gitAUTOINC+590c7d7fe1-g590c7d7fe1« wird verlassen
    make[1]: Verzeichnis »/home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/board-support/u-boot-2017.01+gitAUTOINC+590c7d7fe1-g590c7d7fe1« wird betreten
    CHK include/config/uboot.release
    CHK include/generated/version_autogenerated.h
    CHK include/generated/timestamp_autogenerated.h
    UPD include/generated/timestamp_autogenerated.h
    CHK include/generated/generic-asm-offsets.h
    CHK include/generated/asm-offsets.h
    HOSTCC tools/mkenvimage.o
    HOSTLD tools/mkenvimage
    HOSTCC tools/fit_image.o
    HOSTCC tools/image-host.o
    HOSTCC tools/dumpimage.o
    HOSTLD tools/dumpimage
    HOSTCC tools/mkimage.o
    HOSTLD tools/mkimage
    CC cmd/version.o
    LD cmd/built-in.o
    CC common/main.o
    CC common/board_f.o
    LD common/built-in.o
    CC lib/efi_loader/helloworld.o
    LD lib/efi_loader/helloworld.so
    OBJCOPY lib/efi_loader/helloworld.efi
    CC lib/smbios.o
    CC lib/display_options.o
    LD lib/built-in.o
    LD u-boot
    OBJCOPY u-boot-nodtb.bin
    MKIMAGE u-boot.img
    OBJCOPY u-boot.srec
    CAT u-boot-dtb.bin
    COPY u-boot.bin
    SYM u-boot.sym
    CC spl/common/spl/spl.o
    LD spl/common/spl/built-in.o
    CC spl/lib/display_options.o
    LD spl/lib/built-in.o
    LD spl/u-boot-spl
    /home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-ld.bfd: u-boot-spl section `.rodata' will not fit in region `.sram'
    /home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-ld.bfd: region `.sram' overflowed by 17180 bytes
    common/built-in.o: In Funktion `zm_dprintf':
    /home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/board-support/u-boot-2017.01+gitAUTOINC+590c7d7fe1-g590c7d7fe1/common/xyzModem.c:248: Nicht definierter Verweis auf `vsprintf'
    make[2]: *** [spl/u-boot-spl] Fehler 1
    make[1]: *** [spl/u-boot-spl] Fehler 2
    make[1]: Verzeichnis »/home/eric/ti-processor-sdk-linux-am335x-evm-04.01.00.06/board-support/u-boot-2017.01+gitAUTOINC+590c7d7fe1-g590c7d7fe1« wird verlassen
    make: *** [u-boot] Fehler 2

    Any idea why I get this error? Without the #define debug, I can make the uboot without errors?!

    Kind regards
    Eric
  • `.rodata' will not fit in region `.sram' - you have to run ARCH=arm make menuconfig go to SPL / TPL section and remove some features from MLO to fit the .rodata in .sram

  • Hello Kemal,

    could you please be a little more specific?
    What do you mean by menuconfig?
    Which features should I remove without getting new problems? I couldnt find anything about this in the uboot board port section.

    Thank you for your advise.
    Kind regards

    Eric
  • Remove the features which you don't need and other configurations doesn't depend on it.