This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: Path_config value

Part Number: TMS320C6678


Hi,

The customer configured SRIO working with 1×LaneA and 2×LaneAB, But the values ​​of PLM_SP(n)_PATH_CTL are 1024 and 1025. It seems the value of bit Path_config are always be configured to 4 lanes.

I have found this post https://e2e.ti.com/support/processors/f/791/p/452311/1627862 was the same doubt. And at the end of the post  said Path_config is read only from the user perspective.  It is set by tie-offs at the device level.  Don't attempt to write it.  It should always read '4'.  

Does it mean that the value of Path_config will not be changed regardless of the configuration? Please help give some advice.