Hello all.
I am working on a project where I am looking for very low delay (latency) based RF Communication Microcontroller or SoC. My project is very timing critical and I need to send Data with around 200m (Chip Antenna based design) range with delay time of few microsec level.
My project is a Camera Controller with Wireless Flash trigger. There will be a Master Device (Connected with DSLR Camera Hot-Shoe) and other several (up-to 16) Salve Device (Connected with Flash or SpeedLight. Here Main Device will get signal from Camera Hot-Shoe and do a RF-Broadcast with Control Packet which will be received by nearby (within 200m range) Slave Devices and Trigger the Flash. For this I need to use very low latency/delay based RF Communication.
I don't want to use Bluetooth or WiFi based communication here. I am looking for other RF solution. Also this will be a commercial product so I need to consider the allowed freq for US, Europe etc.
Can anyone advise me a suitable TI RF Microcontroller with the specific feature (or example code) for my application?
Thanks in advance.
Regards.