Hello,
My task is to develop an application package (API) for the TRF372017. Since our system hardware is not ready yet, I may use the TRF372017EVM instead.
Are there any sample code for using the EVM in a separate application?
How is the SPI interface to the TRF controlled from the PC?
Where to get the source code of TRF372017 EVM GUI or parts that describe the control of the TRF372017?
Regards
Melanie