I am trying to load data via SPI onto the LMX2492 PLL registers in order to create a ramp. But I am unaware of exactly how to do it. I have assumed the following about loading data:
If I want to load data 0x15 onto register 0x24 then the 24-bit data packet should be as follows:
0b 0001 0101 0000 0000 0010 0100, where the left-most 0001 0101 represents the 8-bit data 0x15 and the right-most 16-bit data 0000 0000 0010 0100 represents the register address 0x24.
Can anyone confirm that this is the way data is loaded onto appropriate registers?