Hi,
I'm using a TSW38j84 board and have to program the devices using the FMC (JESD) connector. Unfortunately I didn't find a SPI interface to the TRF3722 device in the schematic (Rev B April 03,2014).
There are now two options:
I have an old, erronous schematic downloaded from TI Homepage or
it is indeed impossible to program all devices via FMC
Who can help solving this problem. Thanks in advance.