Hello,
Is the distortion of the LO inputs leaked to the RF output ?
Since there is no PLL in the device, I think that the distortion of the LO inputs leak to the RF output.
Best Regads,
Ryuji Asaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am not sure that I follow what distortions on the LO you are referring. You will see some of the LO signal at the output. This is due to DC imbalance on the baseband inputs and partially to the LO to RF isolation. Optimizing the DC offset balance eliminates the carrier feedthrough performance. If there are LO spurs then that will get "mixed" just like the fundamental itself which leads to distortion on the output.
-RJH
Asaka-san:
Operation with a square wave is OK, though not typical as it is difficult to maintain a true square wave at RF frequencies (as all of the harmonics tend to get heavily attenuated). I do not have any data related to performance with duty cycle variation. My gut feel is that the performance would suffer. I think there would be a spurious offset equivalent to the deviation from ideal (50%).
--Russell