Other Parts Discussed in Thread: FDC1004
I am using the FDC2212, in differential mode with an external 25 MHz oscillator and C0G tank (LC) capacitor, to measure the capacitance of a concentric tube sensor. Overall I am very happy with the sensor, but the measurements change as function of the ambient temperature, even when a fixed capacitor C0G is soldered to the input. The expected change in capacitance from the fixed capacitor is about 0.45 pF, but I am seeing changes of 1.5 pF.
I have confirmed through experimental testing that the composition of the inductor core has an effect on temperature stability of the measurement system, with iron core being the most stable. I then switched the external oscillator from 25 ppm/c to 0.2 ppm/c, but surprisingly, the temperature stability of the system did not improve. My question is: what other factors effect the temperature stability of the measurement system?