Other Parts Discussed in Thread: FDC1004, FDC2214
Tool/software: Starterware
I just bought the FDC1004EVM and it has stopped communicating with the GUI in Windows after a failed attempt to update firmware.
I cannot communicate with it again.
When I plug it in, Windows recognizes it as a USB.
But the GUI does not see it.
It communicated correctly with the GUI initially.
I was trying to update the firmware: I thought perhaps it shipped with an earlier firmware and wanted to update it.
I read the Instructions and was following them in Section 3.9
It started off OK, but then it hung up.
I waited for at least 10 minutes before interrupting the process: I am fully aware of the risks of doing this.
The instructions say it might take some time.
"Wait for the firmware to upload. Do NOT disconnect the EVM from the PC at this time! Also note that the GUI will disconnect from the EVM. The upload process should not take more than one minute. If the upload fails or lasts longer than one minute, unplug the EVM and restart the GUI."
I followed the procedure: disconnected the device and restarted the GUI if upload is not done in more than 1 minute.
i waited 10 minutes.
The device is no longer recognized by the GUI.
What can I do?
Thanks.