Hello,
Can you tell me how the HDC1080 responds when frost builds up on the device? Will it provide a humidity indication? 0%, 100%?
Our application canl be running at -10 deg. F and then when a door opens the chamber where the HDC1080 is located would / could be flooded with humid air causing frost to build on the device.
Will the HDC1080 see the increase in humidity or will it have an error?
I did not find any information on the data sheet concerning frost unless that is considered condensation with the HDC1080.
Thanks,
Len Jenski