We see that the Proximity value and the Measured Sensor Frequency is very sensitive to Sudden Temperature change and that its takes a very long time(+30min) before the measured values stabilize after a sudden Ambient Temperature change of for example +/-45°C (15°C to 60°C) see also below Graphs
Can we do something in our circuitery so that this behaviour is compensated?