Hi everyone,
I have three different applications in which I need respectively at least 2kSps, 10 kSps, 30kSps. I need only L measurment and I would like to have the best possible resolution. Moreover, I would like to use multiple coil.
I know that there are many alternatives like LDC1614, LDC1314 and LDC1000 which have different sample rates. From datasheet I see that LDC1000 has a maximum 78 ksps which is very attractive for my purpose, but from this post http://e2e.ti.com/support/sensor/inductive-sensing/f/938/t/366942 I understand that there is a strong compromise with resolution due to noise. LDC1614/12 and LDC1314/12 have the advantage of multiple coil but probably the sample rate will go down if I use multiple channel.
If I would make a new PCB and use an LDC what is the best choice? The USB interface of the EVM how much decrease the effective sample rate?
Best regards
Alberto