Hello All,
Currently i am working on some PoC where we need to measure the distance between two metallic object (Assume metallic door) moving towards each other, we identified the LDCxxx Series is capable of measuring the distance, however our requirement is for 0.5 mm to 10 mm detecting distance, to be more precise we need to measure the metallic door gap of 4 mm. Please suggest will this sensor would be able to serve the purpose?
If, Yes then what would be the suitable place to mount this sensor module?
we thought of mounting it on the metallic part of the door, however we are not sure whether mounting the sensor on metallic door will create any problem in sensing the distance??