Part Number: LDC1000
Hi,
after collecting a lot of experience with the the LDC1000 and the Eval Board, I finished my first own design. When I did a test in the temperatur chamber of the design, I found out, that the proximity value drifted largely away from the starting value at room temperature, when the enviroment was heated up to 60°C. Hence, the targetposition was not changed.
-> I started to investigate the problem and built a new pcb sensor, double checked the usage of C0G capacitor and measured the resonace frequency over temperature. I found no significant change in resonance or amplitude. So I assumed it is not the resonant circuit itself.
-> I made a setup with the LDC1000 Eval board and the same sensor pcb and put them both into the temperature chamber.
Here I also found a big change in proximity when temperature increased. 2800@21°C to 15000@60°C without moving anything. -> this means, that the same problem occurs with the eval board.
Any hints on this?
Any other experiences to share regarding temperatur dependencies?
Any help is appreciated,
thanks,
Stefan