Hello,
my customer is working on a weight scale with LDC. He wants to glue the coils to the plate with a spacer material in between. This materilal should be flexibel and fast like a spring. Do you have any recommendation?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
my customer is working on a weight scale with LDC. He wants to glue the coils to the plate with a spacer material in between. This materilal should be flexibel and fast like a spring. Do you have any recommendation?
Regards, Holger
Hello Holger,
I'm not clear on the construction that is being proposed - is the sensor PCB supported from the bottom, with the compressible material above the sensors, and the metal surface on the top? If so, we have used 3M EAR open pocket air foams which can compress to <10% of their original volume and then rebound without memory. You may need to find a sufficiently dense version for this application.
Regards,
ChrisO