Other Parts Discussed in Thread: AWR1642, UNIFLASH
Hi,
I rebuilt the people counting demo ccs project in mmwave_industrial_toolbox_2_0_0, successfully got the final image xwr16xx_pcount_lab.bin in pplcount_16xx_mss\Debug, burned it into AWR1642 EVM using uniflash tool, then run the pplcount_demo_gui.exe and pcount_demo_gui.m, but both show the detection points are zero. If run the prebuilt image in mmwave_industrial_toolbox_2_0_0\labs\lab0011-pplcount\lab0011_pplcount_quickstart, it can work well.
As i want to change some parameters for different scenery, it is need to rebuild the project to get new image, would anyone can help try and check if the build image through ccs project can work or not?
Thanks and BR,
Andy