I have an AFE4404 optical sensor and I am trying to read the data directly into memory without the intermediary of the TI software package. Using a Python Package called PySerial, I was able to see that the port was being read but when I went to read from the serial port, I got no data back.
Do you have any recommendations on a library (does not need to be Python specific) that may be able to read through this data?