Hello
Is there any way to check if the AFE4405 is operating in an external clock mode and it is working with an external clock without problems and has not operated with an internal clock?
Is it ok to think that there is no problem if bit [9] OSC_ENABLE = 0 in Register 23h?
When OSC_ENABL = 0 and there is no external clock, will it operate automatically with internal clock?
Best Regards,
Ryuji