Other Parts Discussed in Thread: AFE4405
Hi,
I've tried to capture the signal from wrist using the afe4405 EVM and 2 LED/PD boards(TI board with 2 green LEDs and 6 LEDs(green/red/IR) from Osram.
After trying several times during a few days, I failed to get a valid waveform for any of the LEDs. The result was a flat of 1.2V(Input Voltage) for LED1, LED2 and LED3.
Sometimes only green LED looked working. I guess the following causes:
1) the parameter settings are not correct.
2) I've tried on wrist and at finger. Maybe for finger the signal is too strong, for wrist the signal is too weak.
3) Or even though I pressed it with a reasonable pressure, the light of the LEDs transfered to the PD directly.
Could anybody let me know what's wrong with my settings or methods?
0) app: AFE4405 EVM version 1.0.0 build date 4 20, 2016
1) TX stage: The TX parameters are as follows: LED1 current 23.46mA, LED2 current 4.692mA, LED3 current 4.692mA. 8bit LED current control = 100mA
2) Timing control: Duty cycle is 1%, pulse rate 100Hz (I've tried duty cycle to 10% but didn't work.)
3) RX stages: ENSEPGAIN: checked(TIA_CF 5pF, TIA_GAIN 50k
4) LED probe 1: the TI probe board shipped with the EVM (2 green LED s + 1 PD)
5) LED probe 2: OSRAM LED/PD: Firefly and SFH 22xx for TI AFE4405 (6 G,R, IR LEDs + 1 PD)
Thanks,
Konan Kim